<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: recipe for target 'clean' failed</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638166#M8195</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ivan,&lt;/P&gt;&lt;P&gt;Are you using KDS V3.2.0? From what I know is that the problem comes from the very long command line passed to the rm command: the make file is able to deal with command line length &amp;gt;8192 on Windows, but not the rm command. So it fails.&lt;/P&gt;&lt;P&gt;I have submitted a report in GNU&amp;nbsp; ARM Eclipse, but to my understanding this is not fixed/improved yet.&lt;/P&gt;&lt;P&gt;The easiest workaround is to delete the files in the output (debug) folder directly in the IDE or on the disk if you need to have them cleaned. Otherwise you could ignore that message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Sep 2016 04:00:09 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2016-09-22T04:00:09Z</dc:date>
    <item>
      <title>recipe for target 'clean' failed</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638164#M8193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am getting the following error when I tried to clean my HEXIWEAR project:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="164797_164797.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122259iB40BCF4E7088B4B7/image-size/large?v=v2&amp;amp;px=999" role="button" title="164797_164797.jpg" alt="164797_164797.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ScreenShot093.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5275i57BF1EB8C9E47B05/image-size/large?v=v2&amp;amp;px=999" role="button" title="ScreenShot093.jpg" alt="ScreenShot093.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Looks like it is complained about .elf file. Have someone experienced the same problem? Any idea how to solve it?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 22:15:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638164#M8193</guid>
      <dc:creator>ivanpfarher</dc:creator>
      <dc:date>2016-09-21T22:15:37Z</dc:date>
    </item>
    <item>
      <title>Re: recipe for target 'clean' failed</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638165#M8194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ivan,&lt;/P&gt;&lt;P&gt;Could you please send the project to me , or tell me where can download it .&lt;/P&gt;&lt;P&gt;And which version&amp;nbsp; of KDS do you used , i will test it on my side .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 03:33:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638165#M8194</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-09-22T03:33:38Z</dc:date>
    </item>
    <item>
      <title>Re: recipe for target 'clean' failed</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638166#M8195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ivan,&lt;/P&gt;&lt;P&gt;Are you using KDS V3.2.0? From what I know is that the problem comes from the very long command line passed to the rm command: the make file is able to deal with command line length &amp;gt;8192 on Windows, but not the rm command. So it fails.&lt;/P&gt;&lt;P&gt;I have submitted a report in GNU&amp;nbsp; ARM Eclipse, but to my understanding this is not fixed/improved yet.&lt;/P&gt;&lt;P&gt;The easiest workaround is to delete the files in the output (debug) folder directly in the IDE or on the disk if you need to have them cleaned. Otherwise you could ignore that message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 04:00:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638166#M8195</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-09-22T04:00:09Z</dc:date>
    </item>
    <item>
      <title>Re: recipe for target 'clean' failed</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638167#M8196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using KDS Version: 3.2.0 + GitHUB + Gitkraken. I could clean and built the project before without issues, but after I checked out previews revision code, I start to get this problem.&lt;/P&gt;&lt;P&gt;My real problem is that I do modification in the code but then when I try to debug I don't see the changes, Its like is using and old built's file (or the built's files are not updated). And I suspect that its happend because of this issue with the cleaning.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have deleted the following files and compile again. I will let you know later what happens.&lt;/P&gt;&lt;P&gt;HEXIWEAR_MK64.elf -[arm/le]&lt;/P&gt;&lt;P&gt;HEXIWEAR_MK64.lst&lt;/P&gt;&lt;P&gt;HEXIWEAR_MK64.bin&lt;/P&gt;&lt;P&gt;HEXIWEAR_MK64.map&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 08:29:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638167#M8196</guid>
      <dc:creator>ivanpfarher</dc:creator>
      <dc:date>2016-09-22T08:29:14Z</dc:date>
    </item>
    <item>
      <title>Re: recipe for target 'clean' failed</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638168#M8197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ivan,&lt;/P&gt;&lt;P&gt;if you delete the .elf, then it only will do a relink, not a complete build of all files.&lt;/P&gt;&lt;P&gt;You would have to delete all the object files too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 15:47:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638168#M8197</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-09-22T15:47:33Z</dc:date>
    </item>
    <item>
      <title>Re: recipe for target 'clean' failed</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638169#M8198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you say "object files" do you mean all .o files?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 21:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638169#M8198</guid>
      <dc:creator>ivanpfarher</dc:creator>
      <dc:date>2016-09-22T21:28:48Z</dc:date>
    </item>
    <item>
      <title>Re: recipe for target 'clean' failed</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638170#M8199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find the project here &lt;A class="link-titled" href="https://github.com/ipfarher/HEXIWEAR.git" title="https://github.com/ipfarher/HEXIWEAR.git"&gt;GitHub - ipfarher/HEXIWEAR: HEXIWEAR firmware&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Let me know if you get same issue than me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2016 21:51:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638170#M8199</guid>
      <dc:creator>ivanpfarher</dc:creator>
      <dc:date>2016-09-22T21:51:26Z</dc:date>
    </item>
    <item>
      <title>Re: recipe for target 'clean' failed</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638171#M8200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes. The simplest thing would be that you delete the whole 'debug' output folder.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2016 03:10:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/638171#M8200</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-09-23T03:10:20Z</dc:date>
    </item>
    <item>
      <title>Re: recipe for target 'clean' failed</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/1151684#M10146</link>
      <description>&lt;P&gt;Does it solved, i am having same errors any suggestions.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 16:54:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/1151684#M10146</guid>
      <dc:creator>Anto_jslin_jijo</dc:creator>
      <dc:date>2020-09-10T16:54:40Z</dc:date>
    </item>
    <item>
      <title>Re: recipe for target 'clean' failed</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/1441657#M10210</link>
      <description>&lt;P&gt;amazing thread! my issue about the cleaning solved!&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcdvoiceonline.xyz" target="_self"&gt;https://mcdvoiceonline.xyz&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Apr 2022 12:11:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/recipe-for-target-clean-failed/m-p/1441657#M10210</guid>
      <dc:creator>winedty</dc:creator>
      <dc:date>2022-04-22T12:11:39Z</dc:date>
    </item>
  </channel>
</rss>