<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: Using c++14?</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Using-c-14/m-p/636550#M8182</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I use KDS for windows but I can't reproduce your issue.&lt;/P&gt;&lt;P&gt;Can you please specify your steps of below with screenshot?&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;-- properties -&amp;gt; c/c++ genereal -&amp;gt; preprocessor include paths, macros, etc. -&amp;gt; providers -&amp;gt; cdt gcc built in... -&amp;gt; add "-std=c++14" without quotation marks at the end of the "command to get compiler specs" line&lt;/P&gt;&lt;P&gt;--g++5 installed&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;can you send me the screenshot of error message?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;Best Regards,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;Jennie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Nov 2016 04:21:26 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2016-11-17T04:21:26Z</dc:date>
    <item>
      <title>Using c++14?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Using-c-14/m-p/636549#M8181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;Part of my current K64F project using Kinetis Design Studio under Ubuntu is written in C++, where it uses syntax available since c++14.&lt;/P&gt;&lt;P&gt;I tried a few things, for example:&lt;/P&gt;&lt;P&gt;-- properties -&amp;gt; cross arm c++ compiler -&amp;gt; optimization -&amp;gt; language standard -&amp;gt; next gnu iso c++ (-std=gnu++1y)&lt;/P&gt;&lt;P&gt;-- properties -&amp;gt; c/c++ genereal -&amp;gt; preprocessor include paths, macros, etc. -&amp;gt; providers -&amp;gt; cdt gcc built in... -&amp;gt; add "-std=c++14" without quotation marks at the end of the "command to get compiler specs" line&lt;/P&gt;&lt;P&gt;--g++5 installed&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I still get compile errors. The compiler does not recognize the new language standard. Where do I have to change the setting?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regard and thanks,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Nov 2016 14:55:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Using-c-14/m-p/636549#M8181</guid>
      <dc:creator>michaelkoller</dc:creator>
      <dc:date>2016-11-06T14:55:39Z</dc:date>
    </item>
    <item>
      <title>Re: Using c++14?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Using-c-14/m-p/636550#M8182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I use KDS for windows but I can't reproduce your issue.&lt;/P&gt;&lt;P&gt;Can you please specify your steps of below with screenshot?&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;-- properties -&amp;gt; c/c++ genereal -&amp;gt; preprocessor include paths, macros, etc. -&amp;gt; providers -&amp;gt; cdt gcc built in... -&amp;gt; add "-std=c++14" without quotation marks at the end of the "command to get compiler specs" line&lt;/P&gt;&lt;P&gt;--g++5 installed&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;can you send me the screenshot of error message?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;Best Regards,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;Jennie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Nov 2016 04:21:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Using-c-14/m-p/636550#M8182</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-11-17T04:21:26Z</dc:date>
    </item>
  </channel>
</rss>