<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: openSDA with Segger FRDM K64  in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/openSDA-with-Segger-FRDM-K64/m-p/624636#M8033</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would check with the task manager if there is a gdb (arm-none-eabi-gdb) running, or the Segger J-Link GDB server, and kill them if they are still there (unresponsive). other than that: &lt;A class="link-titled" href="https://mcuoneclipse.com/2014/11/03/debugging-failure-check-list-and-hints/" title="https://mcuoneclipse.com/2014/11/03/debugging-failure-check-list-and-hints/"&gt;Debugging Failure: Check List and Hints | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Apr 2017 15:39:44 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2017-04-19T15:39:44Z</dc:date>
    <item>
      <title>openSDA with Segger FRDM K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/openSDA-with-Segger-FRDM-K64/m-p/624635#M8032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Until now I've been using the segger Jlink flasher cable. I've now working with a new board and went back using the original usb cable with the OpenSDA interface (in the device manager: JLink CDC UART Port). For some reason I cannot connect to the board and flash it.&lt;/P&gt;&lt;P&gt;I've used all the available options (Segger, obviously, PEMicro and OpenOCD), I've tried with the MBED bootloader and the Segger bootloader (also with my old FRDM K64 board and a new FRDM K64 board). I've tried the SWD button as well as the JTAG button (in the SEGGER config window).&lt;/P&gt;&lt;P&gt;Surely I'm doing something wrong..&lt;/P&gt;&lt;P&gt;What have I forgotten?&lt;/P&gt;&lt;P&gt;Using the SEGGER:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Connecting to target...ERROR: Could not connect to target.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Target connection failed. GDBServer will be closed...Restoring target state and closing J-Link connection...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Apr 2017 15:29:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/openSDA-with-Segger-FRDM-K64/m-p/624635#M8032</guid>
      <dc:creator>roymessinger</dc:creator>
      <dc:date>2017-04-19T15:29:44Z</dc:date>
    </item>
    <item>
      <title>Re: openSDA with Segger FRDM K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/openSDA-with-Segger-FRDM-K64/m-p/624636#M8033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would check with the task manager if there is a gdb (arm-none-eabi-gdb) running, or the Segger J-Link GDB server, and kill them if they are still there (unresponsive). other than that: &lt;A class="link-titled" href="https://mcuoneclipse.com/2014/11/03/debugging-failure-check-list-and-hints/" title="https://mcuoneclipse.com/2014/11/03/debugging-failure-check-list-and-hints/"&gt;Debugging Failure: Check List and Hints | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Apr 2017 15:39:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/openSDA-with-Segger-FRDM-K64/m-p/624636#M8033</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-04-19T15:39:44Z</dc:date>
    </item>
  </channel>
</rss>