<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: Breakpoint not working</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Breakpoint-not-working/m-p/614942#M7790</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Biafra,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please create a simple project , which puts some code into SDRAM,&lt;/P&gt;&lt;P&gt;set a breakpoint, then check whether it can stop at that breakpoint .&lt;/P&gt;&lt;P&gt;I test on other chip , it can stop, what about yours.&lt;/P&gt;&lt;P&gt;If yes,&amp;nbsp; next you need analyze your project.&lt;/P&gt;&lt;P&gt;And how many breakpoints in your project,&amp;nbsp; please first delete others to have a try .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jan 2017 08:18:31 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2017-01-17T08:18:31Z</dc:date>
    <item>
      <title>Breakpoint not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Breakpoint-not-working/m-p/614941#M7789</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;posted another question about loading an application to debug in SDRAM in the post&amp;nbsp;&lt;A _jive_internal="true" data-containerid="11213" data-containertype="14" data-objectid="442023" data-objecttype="1" href="https://community.nxp.com/thread/442023"&gt;Debug in SDRAM&lt;/A&gt;&amp;nbsp;referred to summarize the basic steps.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I'm working on a custom board based on K65FX1M0M18 using KDS 3.2.0 and Multilink Universal debugger.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;In the board there are:&lt;/P&gt;&lt;UL&gt;&lt;LI style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN&gt;K65F&lt;/SPAN&gt;&lt;SPAN&gt;X&lt;/SPAN&gt;&lt;SPAN&gt;1&lt;/SPAN&gt;&lt;SPAN&gt;M0M18 &lt;/SPAN&gt;&lt;/LI&gt;&lt;LI style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN style="background-color: #ffffff;"&gt;External SDRAM (4M x 32)&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN style="background-color: #ffffff;"&gt;External flash&amp;nbsp;(2M x 16),&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P style="min-height: 8pt; padding: 0px; color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;At this time I'm using the following workflow (anomalous for me):&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I open the application project in KDS&lt;/LI&gt;&lt;LI&gt;I build the application linked at&amp;nbsp;SDRAM address&lt;/LI&gt;&lt;LI&gt;Using the bootloader in runtime environment I load the application just built in the external flash memory&lt;/LI&gt;&lt;LI&gt;I run the debugger that resets the&amp;nbsp;K65 (starting at the startup address 0), so the bootloader starts and copies the application from the external flash to external SDRAM. As long as the booloader is running, I can step without source files, but when it jumps to the application I can see the application source files too&lt;/LI&gt;&lt;/UL&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tested the runtime behaviour and it works well: a sample application that flashes a led runs as expected.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The problem rises in the debugging phase: although I can step in the application, if I set a breakpoint and run, the program doesn't stop until I press the stop button in the debugger, even if the breakpoint is set in the line following the current one.&lt;/P&gt;&lt;P&gt;The breakpoint seems to work only if it is set in the bootloader area.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone have experienced this or has any suggestion on it?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Biafra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 15:50:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Breakpoint-not-working/m-p/614941#M7789</guid>
      <dc:creator>biafra</dc:creator>
      <dc:date>2017-01-13T15:50:20Z</dc:date>
    </item>
    <item>
      <title>Re: Breakpoint not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Breakpoint-not-working/m-p/614942#M7790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Biafra,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please create a simple project , which puts some code into SDRAM,&lt;/P&gt;&lt;P&gt;set a breakpoint, then check whether it can stop at that breakpoint .&lt;/P&gt;&lt;P&gt;I test on other chip , it can stop, what about yours.&lt;/P&gt;&lt;P&gt;If yes,&amp;nbsp; next you need analyze your project.&lt;/P&gt;&lt;P&gt;And how many breakpoints in your project,&amp;nbsp; please first delete others to have a try .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2017 08:18:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Breakpoint-not-working/m-p/614942#M7790</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-01-17T08:18:31Z</dc:date>
    </item>
  </channel>
</rss>