<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: Program blank MK64F from FRDM board</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-blank-MK64F-from-FRDM-board/m-p/606454#M7626</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;thanks for your quick answer XD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, I didn't mean that I replaced the existing chip, but the situation is pretty much the same as I'm trying to write the content of a brand new device.&lt;/P&gt;&lt;P&gt;I copied the pinout of the existing SWD connector and pasted it to a new board. I used the FRDM to develop a prototype of the firmware to be loaded into the new chip, needless to say that the code is exactly the same, otherwise I would have a different kind of error (device not supported or something similar).&lt;/P&gt;&lt;P&gt;The "old" chip is still programming and working fine, but the "new" one has this problem.&lt;/P&gt;&lt;P&gt;The FRDM programming chip has the latest MBED bootloader as I thought this might have solved this.&lt;/P&gt;&lt;P&gt;I will try to change the bootloader FW to the Jlink as soon as possible and see if this fixes the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again for your answer.&lt;/P&gt;&lt;P&gt;Have a nice day,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Tommaso&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Feb 2017 08:46:03 GMT</pubDate>
    <dc:creator>tommyb90</dc:creator>
    <dc:date>2017-02-07T08:46:03Z</dc:date>
    <item>
      <title>Program blank MK64F from FRDM board</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-blank-MK64F-from-FRDM-board/m-p/606452#M7624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a problem while programming a blank MK64F.&lt;/P&gt;&lt;P&gt;I bought a blank micro to be embedded into another circuit. Once soldered I wanted to load the program using the FRDM-K64F board that I used to develop the firmware.&lt;/P&gt;&lt;P&gt;At this point using OpenSDA the procedure fails and using MBED I get this error:&lt;/P&gt;&lt;P&gt;"The interface firmware FAILED to reset/halt the target MCU".&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think this is relative to the RESET pin oscillating as the micro is blank. Is there a way to avoid this and program the chip anyway?&lt;/P&gt;&lt;P&gt;Has anybody had the same issue?&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Tommaso&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 15:34:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-blank-MK64F-from-FRDM-board/m-p/606452#M7624</guid>
      <dc:creator>tommyb90</dc:creator>
      <dc:date>2017-02-06T15:34:10Z</dc:date>
    </item>
    <item>
      <title>Re: Program blank MK64F from FRDM board</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-blank-MK64F-from-FRDM-board/m-p/606453#M7625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tommaso,&lt;/P&gt;&lt;P&gt;Do you meaning replace the MK64 chip which on FRDM-K64 board with a new chip ?&lt;/P&gt;&lt;P&gt;If yes, first please check the part number of the new chip, when download program ,&lt;/P&gt;&lt;P&gt;select the right chip . Second , you can change the firmware to Jlink to have a try.&lt;/P&gt;&lt;P&gt;If you want use the FRDM-K64 to debug other board, there is a tutorial you can refer to :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/" title="https://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/"&gt;Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 02:48:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-blank-MK64F-from-FRDM-board/m-p/606453#M7625</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-02-07T02:48:23Z</dc:date>
    </item>
    <item>
      <title>Re: Program blank MK64F from FRDM board</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-blank-MK64F-from-FRDM-board/m-p/606454#M7626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;thanks for your quick answer XD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, I didn't mean that I replaced the existing chip, but the situation is pretty much the same as I'm trying to write the content of a brand new device.&lt;/P&gt;&lt;P&gt;I copied the pinout of the existing SWD connector and pasted it to a new board. I used the FRDM to develop a prototype of the firmware to be loaded into the new chip, needless to say that the code is exactly the same, otherwise I would have a different kind of error (device not supported or something similar).&lt;/P&gt;&lt;P&gt;The "old" chip is still programming and working fine, but the "new" one has this problem.&lt;/P&gt;&lt;P&gt;The FRDM programming chip has the latest MBED bootloader as I thought this might have solved this.&lt;/P&gt;&lt;P&gt;I will try to change the bootloader FW to the Jlink as soon as possible and see if this fixes the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again for your answer.&lt;/P&gt;&lt;P&gt;Have a nice day,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Tommaso&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 08:46:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-blank-MK64F-from-FRDM-board/m-p/606454#M7626</guid>
      <dc:creator>tommyb90</dc:creator>
      <dc:date>2017-02-07T08:46:03Z</dc:date>
    </item>
    <item>
      <title>Re: Program blank MK64F from FRDM board</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-blank-MK64F-from-FRDM-board/m-p/606455#M7627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, sorry for the late reply.&lt;/P&gt;&lt;P&gt;Unfortunately the Jlink bootloader didn't work either. Same issue.&lt;/P&gt;&lt;P&gt;I made some other tests, though: I had the opportunity to use a Multilink universal by borrowing one and one thing I found out is that I'm not able to program the chip via SWD, but with JTAG programming this works perfectly.&lt;/P&gt;&lt;P&gt;Then I thought that, once programmed, the issue with the SWD would not be a problem. I was wrong, at this point I can only program the chip via JTAG and not via SWD. I'm lost.&lt;/P&gt;&lt;P&gt;Needless to say that the pins are working because the same pinout used in SWD is used in a different manner in JTAG, so every link to the uC is working fine.&lt;/P&gt;&lt;P&gt;I'm the only one who is facing this problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Tommaso&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Feb 2017 07:12:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-blank-MK64F-from-FRDM-board/m-p/606455#M7627</guid>
      <dc:creator>tommyb90</dc:creator>
      <dc:date>2017-02-13T07:12:29Z</dc:date>
    </item>
    <item>
      <title>Re: Program blank MK64F from FRDM board</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-blank-MK64F-from-FRDM-board/m-p/606456#M7628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tommaso,&lt;/P&gt;&lt;P&gt;About SWD interface, there is a design on FRDM board as Erich shows :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/793145"&gt;https://community.nxp.com/message/793145&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please refer to it check yours .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;ALice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2017 03:00:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-blank-MK64F-from-FRDM-board/m-p/606456#M7628</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-02-15T03:00:03Z</dc:date>
    </item>
    <item>
      <title>Re: Program blank MK64F from FRDM board</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-blank-MK64F-from-FRDM-board/m-p/606457#M7629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;no success until now.&lt;/P&gt;&lt;P&gt;I checked the wiring and the HW, the bootloader is able to program the embedded uC, but not the one on the board.&lt;/P&gt;&lt;P&gt;The wiring is absolutely the same.&lt;/P&gt;&lt;P&gt;I also checked the EZ port, the JTAG TDI and TDO pins and the NMI (I added pullups on those to be sure).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything else that could stop the programming of the device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Tommaso&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Feb 2017 14:29:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-blank-MK64F-from-FRDM-board/m-p/606457#M7629</guid>
      <dc:creator>tommyb90</dc:creator>
      <dc:date>2017-02-23T14:29:56Z</dc:date>
    </item>
  </channel>
</rss>