<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックemWin Library on KDS</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/emWin-Library-on-KDS/m-p/606434#M7622</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I would like to evaluate emWin precompiled library from NXP. Now, I am working with KDS 3.2.0 and a custom board with a MK22FN1M MCU and RGB display with an external (parallel interface) controller, SSD1961. Is it possible to link the library under KDS with GNU toolchain (arm-none-eabi-gcc) and to run it with that MCU ?. In that case, which library must be used? The one precompiled with LPCXpresso (libemWin_M4F.a) ?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Sep 2016 17:37:41 GMT</pubDate>
    <dc:creator>antoinelorenz</dc:creator>
    <dc:date>2016-09-09T17:37:41Z</dc:date>
    <item>
      <title>emWin Library on KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/emWin-Library-on-KDS/m-p/606434#M7622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I would like to evaluate emWin precompiled library from NXP. Now, I am working with KDS 3.2.0 and a custom board with a MK22FN1M MCU and RGB display with an external (parallel interface) controller, SSD1961. Is it possible to link the library under KDS with GNU toolchain (arm-none-eabi-gcc) and to run it with that MCU ?. In that case, which library must be used? The one precompiled with LPCXpresso (libemWin_M4F.a) ?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2016 17:37:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/emWin-Library-on-KDS/m-p/606434#M7622</guid>
      <dc:creator>antoinelorenz</dc:creator>
      <dc:date>2016-09-09T17:37:41Z</dc:date>
    </item>
    <item>
      <title>Re: emWin Library on KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/emWin-Library-on-KDS/m-p/606435#M7623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Abtoine,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- I have&amp;nbsp; not used emWin library , while i checked one customer use it on KDS :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/385566"&gt;linker errors "multiple defintion of" when migrating from KDS 2.0 to 3.1&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- There is a emWin User Guide :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.nxp.com/files/microcontrollers/doc/support_info/UM03001_emWin5_7.pdf?fsrch=1&amp;amp;sr=2&amp;amp;pageNum=1" title="http://cache.nxp.com/files/microcontrollers/doc/support_info/UM03001_emWin5_7.pdf?fsrch=1&amp;amp;sr=2&amp;amp;pageNum=1"&gt;http://cache.nxp.com/files/microcontrollers/doc/support_info/UM03001_emWin5_7.pdf?fsrch=1&amp;amp;sr=2&amp;amp;pageNum=1&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can especially check the part of "2 Getting Started" .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- In KDS, if you want add library , please right click your project, select "Properties" ,&lt;/P&gt;&lt;P&gt;then :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5092i165F0D07CCD28FA6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it&amp;nbsp; helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 03:15:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/emWin-Library-on-KDS/m-p/606435#M7623</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-09-13T03:15:02Z</dc:date>
    </item>
  </channel>
</rss>