<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Undefined reference in KDS 3.2 in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Undefined-reference-in-KDS-3-2/m-p/603072#M7585</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Slavko Radovic&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you share screen shots of the build configuration of the project that do not delete the *.o files?&lt;/P&gt;&lt;P&gt;project folder(righ click)-&amp;gt;properties-&amp;gt;C/C++ Build-&amp;gt;(Tab)Behavior&lt;/P&gt;&lt;P&gt;project folder(righ click)-&amp;gt;properties-&amp;gt;Sttings-&amp;gt;(Tab)Toolchains&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure that this configuration is as the follow&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3779i71691CBA87F9514B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3720i63C188F154F77F72/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Oct 2016 23:56:18 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2016-10-11T23:56:18Z</dc:date>
    <item>
      <title>Undefined reference in KDS 3.2</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Undefined-reference-in-KDS-3-2/m-p/603071#M7584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm having problem with building and cleaning the project&lt;/P&gt;&lt;P&gt;If I do it with settings in file .cproject_ok it build ok, but when I try to clean I have this message:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;make clean &lt;BR /&gt;rm&amp;nbsp; si_o_app.siz&amp;nbsp; ./src/board_ub_iritel/board.o ./src/board_ub_iritel/gpio_pins.o ./src/board_ub_iritel/pin_mux.o&amp;nbsp; ./src/MQX/app_mqx.o&amp;nbsp; ./src/Interrupt_Handler/fsl_dspi_irq.o ./src/Interrupt_Handler/fsl_edma_irq.o ./src/Interrupt_Handler/fsl_ftm_irq.o ./src/Interrupt_Handler/fsl_sai_irq.o ./src/Interrupt_Handler/i2c_mqx_rtos_irq.o&amp;nbsp; ./src/BSP_Files/hardware_init.o ./src/BSP_Files/init_bsp.o ./src/BSP_Files/mqx_main.o&amp;nbsp; ./src/Audio/WM8731_driver.o ./src/Audio/audio.o ./src/Audio/fsl_soundcard.o ./src/Audio/main_call.o ./src/Audio/rtp.o&amp;nbsp; ./src/alarm.o ./src/config.o ./src/ethernet.o ./src/events.o ./src/headset.o ./src/init.o ./src/led.o ./src/main_call.o ./src/main_task.o ./src/si_o_main.o ./src/signalling.o ./src/spi.o&amp;nbsp; ./src/board_ub_iritel/board.d ./src/board_ub_iritel/gpio_pins.d ./src/board_ub_iritel/pin_mux.d&amp;nbsp; ./src/MQX/app_mqx.d&amp;nbsp; ./src/Interrupt_Handler/fsl_dspi_irq.d ./src/Interrupt_Handler/fsl_edma_irq.d ./src/Interrupt_Handler/fsl_ftm_irq.d ./src/Interrupt_Handler/fsl_sai_irq.d ./src/Interrupt_Handler/i2c_mqx_rtos_irq.d&amp;nbsp; ./src/BSP_Files/hardware_init.d ./src/BSP_Files/init_bsp.d ./src/BSP_Files/mqx_main.d&amp;nbsp; ./src/Audio/WM8731_driver.d ./src/Audio/audio.d ./src/Audio/fsl_soundcard.d ./src/Audio/main_call.d ./src/Audio/rtp.d&amp;nbsp; ./src/alarm.d ./src/config.d ./src/ethernet.d ./src/events.d ./src/headset.d ./src/init.d ./src/led.d ./src/main_call.d ./src/main_task.d ./src/si_o_main.d ./src/signalling.d ./src/spi.d&amp;nbsp; si_o_app.hex&amp;nbsp; si_o_app.elf&lt;BR /&gt;rm: cannot remove 'si_o_app.siz': No such file or directory&lt;BR /&gt;rm: cannot remove 'si_o_app.hex': No such file or directory&lt;BR /&gt;make: [clean] Error 1 (ignored)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;In win it doesn't delete *.o files&amp;nbsp;(you must do it manually), but in linux it does.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I do it with settings in file .cproject_nok it won't build, I have this message (I put only one error but most of them are something like ENET_DRV_X, ENET_HAL_X and UART_DRV_X):&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;SDK_1.3_MK64FN1M012/middleware/tcpip/rtcs/lib/frdmk64f.kds/debug/rtcs/lib_rtcs.a(fsl_enet_rtcs_adapter.o): In function `enet_send':&lt;/P&gt;&lt;P&gt;SDK_1.3_MK64FN1M012/middleware/tcpip/rtcs/source/port/fsl_enet_rtcs_adapter.h:435: undefined reference to `ENET_DRV_SendData'&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I define in Linker library (_rtcs) and correct path for that library.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And if I try to clean, it's done right with message:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;make clean &lt;BR /&gt;rm -rf&amp;nbsp; si_o_app.siz&amp;nbsp; ./src/board_ub_iritel/board.o ./src/board_ub_iritel/gpio_pins.o ./src/board_ub_iritel/pin_mux.o&amp;nbsp; ./src/MQX/app_mqx.o&amp;nbsp; ./src/Interrupt_Handler/fsl_dspi_irq.o ./src/Interrupt_Handler/fsl_edma_irq.o ./src/Interrupt_Handler/fsl_ftm_irq.o ./src/Interrupt_Handler/fsl_sai_irq.o ./src/Interrupt_Handler/i2c_mqx_rtos_irq.o&amp;nbsp; ./src/BSP_Files/hardware_init.o ./src/BSP_Files/init_bsp.o ./src/BSP_Files/mqx_main.o&amp;nbsp; ./src/Audio/WM8731_driver.o ./src/Audio/audio.o ./src/Audio/fsl_soundcard.o ./src/Audio/main_call.o ./src/Audio/rtp.o&amp;nbsp; ./src/alarm.o ./src/config.o ./src/ethernet.o ./src/events.o ./src/headset.o ./src/init.o ./src/led.o ./src/main_call.o ./src/main_task.o ./src/si_o_main.o ./src/signalling.o ./src/spi.o&amp;nbsp; ./src/board_ub_iritel/board.d ./src/board_ub_iritel/gpio_pins.d ./src/board_ub_iritel/pin_mux.d&amp;nbsp; ./src/MQX/app_mqx.d&amp;nbsp; ./src/Interrupt_Handler/fsl_dspi_irq.d ./src/Interrupt_Handler/fsl_edma_irq.d ./src/Interrupt_Handler/fsl_ftm_irq.d ./src/Interrupt_Handler/fsl_sai_irq.d ./src/Interrupt_Handler/i2c_mqx_rtos_irq.d&amp;nbsp; ./src/BSP_Files/hardware_init.d ./src/BSP_Files/init_bsp.d ./src/BSP_Files/mqx_main.d&amp;nbsp; ./src/Audio/WM8731_driver.d ./src/Audio/audio.d ./src/Audio/fsl_soundcard.d ./src/Audio/main_call.d ./src/Audio/rtp.d&amp;nbsp; ./src/alarm.d ./src/config.d ./src/ethernet.d ./src/events.d ./src/headset.d ./src/init.d ./src/led.d ./src/main_call.d ./src/main_task.d ./src/si_o_main.d ./src/signalling.d ./src/spi.d&amp;nbsp; si_o_app.hex&amp;nbsp; si_o_app.elf&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338949"&gt;.cproject_ok.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338949"&gt;.cproject_nok.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Oct 2016 13:52:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Undefined-reference-in-KDS-3-2/m-p/603071#M7584</guid>
      <dc:creator>slavko1001</dc:creator>
      <dc:date>2016-10-04T13:52:33Z</dc:date>
    </item>
    <item>
      <title>Re: Undefined reference in KDS 3.2</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Undefined-reference-in-KDS-3-2/m-p/603072#M7585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Slavko Radovic&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you share screen shots of the build configuration of the project that do not delete the *.o files?&lt;/P&gt;&lt;P&gt;project folder(righ click)-&amp;gt;properties-&amp;gt;C/C++ Build-&amp;gt;(Tab)Behavior&lt;/P&gt;&lt;P&gt;project folder(righ click)-&amp;gt;properties-&amp;gt;Sttings-&amp;gt;(Tab)Toolchains&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure that this configuration is as the follow&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3779i71691CBA87F9514B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3720i63C188F154F77F72/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Oct 2016 23:56:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Undefined-reference-in-KDS-3-2/m-p/603072#M7585</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2016-10-11T23:56:18Z</dc:date>
    </item>
  </channel>
</rss>