<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: Post-Build Failure, Unterminated Quoted String</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Post-Build-Failure-Unterminated-Quoted-String/m-p/600690#M7554</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi Phil,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you post a screenshot of your post build command? Have you tried renaming the folder to "PS600_Firmware"?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Dec 2016 18:25:47 GMT</pubDate>
    <dc:creator>Carlos_Mendoza</dc:creator>
    <dc:date>2016-12-13T18:25:47Z</dc:date>
    <item>
      <title>Post-Build Failure, Unterminated Quoted String</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Post-Build-Failure-Unterminated-Quoted-String/m-p/600689#M7553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Although the code compiles and works properly, I get a post-build syntax error that has me worried. &amp;nbsp;Here is what I see:&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;make --no-print-directory post-build&lt;BR /&gt;"C:/Users/Phil/Dropbox/Development/PS600 Firmware/CM601/Applications/uTaskerV1.4/KinetisDesignStudio/uTaskerV1.4_FLASH/generate.bat&lt;BR /&gt;c:/freescale/kds_v3/eclipse/../bin/sh: syntax error: unterminated quoted string&lt;BR /&gt;makefile:97: recipe for target 'post-build' failed&lt;BR /&gt;make[1]: [post-build] Error 2 (ignored)&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(see attached file for complete console compile log)&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am suspecting that the error has something to do with my directory name having a space in the name. "PS600 Firmware"? &amp;nbsp;If this directory structure is put in the path, is it possible that the error happen with the improper PATH formation?&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any&amp;nbsp;suggestions?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338944"&gt;post-build-failure-compile.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 10 Dec 2016 23:00:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Post-Build-Failure-Unterminated-Quoted-String/m-p/600689#M7553</guid>
      <dc:creator>philhale</dc:creator>
      <dc:date>2016-12-10T23:00:48Z</dc:date>
    </item>
    <item>
      <title>Re: Post-Build Failure, Unterminated Quoted String</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Post-Build-Failure-Unterminated-Quoted-String/m-p/600690#M7554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi Phil,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you post a screenshot of your post build command? Have you tried renaming the folder to "PS600_Firmware"?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 18:25:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Post-Build-Failure-Unterminated-Quoted-String/m-p/600690#M7554</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2016-12-13T18:25:47Z</dc:date>
    </item>
    <item>
      <title>Re: Post-Build Failure, Unterminated Quoted String</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Post-Build-Failure-Unterminated-Quoted-String/m-p/600691#M7555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9644iEF3931673CF8BE17/image-size/large?v=v2&amp;amp;px=999" title="ScreenHunter_262 Dec. 13 10.41.jpg" alt="ScreenHunter_262 Dec. 13 10.41.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, I have not tried to rename the folder. I am worried it may cause other problems and I have numerous other applications in the same directory that work fine. This is the first occurrence of this problem that I can tell.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 18:43:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Post-Build-Failure-Unterminated-Quoted-String/m-p/600691#M7555</guid>
      <dc:creator>philhale</dc:creator>
      <dc:date>2016-12-13T18:43:39Z</dc:date>
    </item>
    <item>
      <title>Re: Post-Build Failure, Unterminated Quoted String</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Post-Build-Failure-Unterminated-Quoted-String/m-p/600692#M7556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Phil&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the build steps tab there is a post-build command doing something like this:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;"${ProjDirPath}/Applications/uTaskerV1.4/KinetisDesignStudio/uTaskerV1.4_FLASH/generate.bat&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is calling a bat file to generate various output formats (because KDS can't select more than one at a time) and possibly also combining the file file with a boot loader, and/or encrypting it).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Notice that the line starts with &lt;STRONG&gt;"&lt;/STRONG&gt; but there is no terminating one - like&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;"${ProjDirPath}/Applications/uTaskerV1.4/KinetisDesignStudio/uTaskerV1.4_FLASH/generate.bat&lt;SPAN style="color: #ff0000;"&gt;"&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This was not a problem with previous KDS versions but KDS 3.2.0 doesn't like it. If you add the terminating &lt;STRONG&gt;"&lt;/STRONG&gt; it will be OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;EM&gt;P.S. If you load and debug in KDS you don't need the output conversions and this error is not actually stopping anything from working...&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 00:54:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Post-Build-Failure-Unterminated-Quoted-String/m-p/600692#M7556</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-12-14T00:54:03Z</dc:date>
    </item>
    <item>
      <title>Re: Post-Build Failure, Unterminated Quoted String</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Post-Build-Failure-Unterminated-Quoted-String/m-p/600693#M7557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That solved the problem! &amp;nbsp;Thank you, Mark!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 17:06:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Post-Build-Failure-Unterminated-Quoted-String/m-p/600693#M7557</guid>
      <dc:creator>philhale</dc:creator>
      <dc:date>2016-12-14T17:06:39Z</dc:date>
    </item>
  </channel>
</rss>