<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: printf() not working in KDS</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-not-working-in-KDS/m-p/592631#M7457</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Martin,&lt;/P&gt;&lt;P&gt;The&amp;nbsp; KDS v3.2 and V3.0 is different with KDS v2.0 , the library is different .&lt;/P&gt;&lt;P&gt;So, on KDS v3.2 and V3.0 , please change the lib to&lt;/P&gt;&lt;P&gt;&lt;EM&gt;-specs=&lt;SPAN class="skimlinks-unlinked"&gt;rdimon.specs&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;SPAN class="skimlinks-unlinked"&gt;&lt;IMG alt="Semihosting Enabled in KDS v3.0.0" class="size-full wp-image-15075 jive-image" height="591" src="https://mcuoneclipse.files.wordpress.com/2015/05/semihosting-enabled-in-kds-v3-0-0.png?w=846&amp;amp;h=857" width="584" /&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;My that DOC is refer to KDS v2.0 , at that time , there is no V3.0&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Aug 2016 13:09:28 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2016-08-12T13:09:28Z</dc:date>
    <item>
      <title>printf() not working in KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-not-working-in-KDS/m-p/592628#M7454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I know that this question has already been answered a lot of time, but it still doesn't work for me.&lt;/P&gt;&lt;P&gt;I am using processor expert and changed the heap size in my processor expert component as indicated in Alice Yang "How to use printf() to print string to Console and UART in KDS" tutorial.&lt;/P&gt;&lt;P&gt;But I can't see anything displayed in the console view.&lt;/P&gt;&lt;P&gt;I know using printf isn't a good practice in embedded, but still I would like to see it working.&lt;/P&gt;&lt;P&gt;If anyone can help, would be grateful !&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 15:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-not-working-in-KDS/m-p/592628#M7454</guid>
      <dc:creator>martinboton</dc:creator>
      <dc:date>2016-08-11T15:00:11Z</dc:date>
    </item>
    <item>
      <title>Re: printf() not working in KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-not-working-in-KDS/m-p/592629#M7455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Martin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please tell me the&amp;nbsp; version of KDS, and which chip .&lt;/P&gt;&lt;P&gt;What about the project , Only with PE ? or with SDK ? or with MQX?&lt;/P&gt;&lt;P&gt;You'd better create one simple project to me , i will check it on my side .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Aug 2016 01:53:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-not-working-in-KDS/m-p/592629#M7455</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-08-12T01:53:39Z</dc:date>
    </item>
    <item>
      <title>Re: printf() not working in KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-not-working-in-KDS/m-p/592630#M7456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use KDS v3.2.0, my project is only with PE, no SDK and no MQX, and I work with a FRDM k64f board.&lt;/P&gt;&lt;P&gt;I attached a simple project so you can check it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Aug 2016 07:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-not-working-in-KDS/m-p/592630#M7456</guid>
      <dc:creator>martinboton</dc:creator>
      <dc:date>2016-08-12T07:56:01Z</dc:date>
    </item>
    <item>
      <title>Re: printf() not working in KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-not-working-in-KDS/m-p/592631#M7457</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Martin,&lt;/P&gt;&lt;P&gt;The&amp;nbsp; KDS v3.2 and V3.0 is different with KDS v2.0 , the library is different .&lt;/P&gt;&lt;P&gt;So, on KDS v3.2 and V3.0 , please change the lib to&lt;/P&gt;&lt;P&gt;&lt;EM&gt;-specs=&lt;SPAN class="skimlinks-unlinked"&gt;rdimon.specs&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;SPAN class="skimlinks-unlinked"&gt;&lt;IMG alt="Semihosting Enabled in KDS v3.0.0" class="size-full wp-image-15075 jive-image" height="591" src="https://mcuoneclipse.files.wordpress.com/2015/05/semihosting-enabled-in-kds-v3-0-0.png?w=846&amp;amp;h=857" width="584" /&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;My that DOC is refer to KDS v2.0 , at that time , there is no V3.0&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Aug 2016 13:09:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-not-working-in-KDS/m-p/592631#M7457</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-08-12T13:09:28Z</dc:date>
    </item>
  </channel>
</rss>