<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックChange target processor in KDS 3.2.0 ?</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Change-target-processor-in-KDS-3-2-0/m-p/573825#M7316</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; I am using the KDS 3.2.0 and currently have nice working project built using the processor expert based on the MKE202Z64VLC4.&amp;nbsp; I want to change it from this 64K Flash memory part to the MKE202Z16VLC4 version (which is the 16K variant).&amp;nbsp;&amp;nbsp; However, I have not found a way to change it.&amp;nbsp; The two devices are the same with the exception of the 16K versus 64K one.&amp;nbsp;&amp;nbsp; Is there a way to change it in the KDS?&amp;nbsp; (It would be time consuming to start all over again).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Jun 2016 18:49:39 GMT</pubDate>
    <dc:creator>blsousan</dc:creator>
    <dc:date>2016-06-24T18:49:39Z</dc:date>
    <item>
      <title>Change target processor in KDS 3.2.0 ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Change-target-processor-in-KDS-3-2-0/m-p/573825#M7316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; I am using the KDS 3.2.0 and currently have nice working project built using the processor expert based on the MKE202Z64VLC4.&amp;nbsp; I want to change it from this 64K Flash memory part to the MKE202Z16VLC4 version (which is the 16K variant).&amp;nbsp;&amp;nbsp; However, I have not found a way to change it.&amp;nbsp; The two devices are the same with the exception of the 16K versus 64K one.&amp;nbsp;&amp;nbsp; Is there a way to change it in the KDS?&amp;nbsp; (It would be time consuming to start all over again).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2016 18:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Change-target-processor-in-KDS-3-2-0/m-p/573825#M7316</guid>
      <dc:creator>blsousan</dc:creator>
      <dc:date>2016-06-24T18:49:39Z</dc:date>
    </item>
    <item>
      <title>Re: Change target processor in KDS 3.2.0 ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Change-target-processor-in-KDS-3-2-0/m-p/573826#M7317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can change the pinout in the CPU component like this: &lt;A href="https://mcuoneclipse.com/2012/08/16/changing-the-cpu-with-processor-expert/" title="https://mcuoneclipse.com/2012/08/16/changing-the-cpu-with-processor-expert/"&gt;https://mcuoneclipse.com/2012/08/16/changing-the-cpu-with-processor-expert/&lt;/A&gt;&amp;nbsp; (description for ColdFire, but same applies to Kinetis/ARM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another one on this subject is here: &lt;A href="https://mcuoneclipse.com/2016/06/25/switching-the-microcontroller-package-device-and-family/" title="https://mcuoneclipse.com/2016/06/25/switching-the-microcontroller-package-device-and-family/"&gt;https://mcuoneclipse.com/2016/06/25/switching-the-microcontroller-package-device-and-family/&lt;/A&gt; &lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Jun 2016 08:23:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Change-target-processor-in-KDS-3-2-0/m-p/573826#M7317</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-06-25T08:23:22Z</dc:date>
    </item>
  </channel>
</rss>