<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 I2C Slave Send not working as expected</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/I2C-Slave-Send-not-working-as-expected/m-p/334186#M716</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got a project with a KLZ05 and I'm trying to use the PE code manage the I2C interface.&amp;nbsp; Device is configured in slave mode and I can send data to the micro without any problems.&amp;nbsp; My difficulty is reading from KLZ05 in slave mode.&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I get to a valid CI2C1_OnReadReq event which means the CPU saw the incoming address and the read read bit.&amp;nbsp; In that event handler routine I call CI2C1_SendChar() provide the send data to the I2C interface in response to the read request.&amp;nbsp; I never see any valid read data on the master side.&amp;nbsp; What is interesting is that I do see the last byte written to the KLZ05 as my read data.&amp;nbsp; I think this means that the host is just reading back the data register of the I2C controller. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there something i need to do to enable the PE code to feed the TX data to the I2C interface beyond calling the CI2C1_SendChar() routine?&amp;nbsp;&amp;nbsp;&amp;nbsp; Some good examples would be a big help.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Feb 2015 20:31:36 GMT</pubDate>
    <dc:creator>DavidLundquist</dc:creator>
    <dc:date>2015-02-24T20:31:36Z</dc:date>
    <item>
      <title>I2C Slave Send not working as expected</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/I2C-Slave-Send-not-working-as-expected/m-p/334186#M716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got a project with a KLZ05 and I'm trying to use the PE code manage the I2C interface.&amp;nbsp; Device is configured in slave mode and I can send data to the micro without any problems.&amp;nbsp; My difficulty is reading from KLZ05 in slave mode.&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I get to a valid CI2C1_OnReadReq event which means the CPU saw the incoming address and the read read bit.&amp;nbsp; In that event handler routine I call CI2C1_SendChar() provide the send data to the I2C interface in response to the read request.&amp;nbsp; I never see any valid read data on the master side.&amp;nbsp; What is interesting is that I do see the last byte written to the KLZ05 as my read data.&amp;nbsp; I think this means that the host is just reading back the data register of the I2C controller. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there something i need to do to enable the PE code to feed the TX data to the I2C interface beyond calling the CI2C1_SendChar() routine?&amp;nbsp;&amp;nbsp;&amp;nbsp; Some good examples would be a big help.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Feb 2015 20:31:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/I2C-Slave-Send-not-working-as-expected/m-p/334186#M716</guid>
      <dc:creator>DavidLundquist</dc:creator>
      <dc:date>2015-02-24T20:31:36Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Slave Send not working as expected</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/I2C-Slave-Send-not-working-as-expected/m-p/334187#M717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Never mind.&amp;nbsp; The PE code is doing exactly what it should.&amp;nbsp; Android host is not.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2015 16:23:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/I2C-Slave-Send-not-working-as-expected/m-p/334187#M717</guid>
      <dc:creator>DavidLundquist</dc:creator>
      <dc:date>2015-02-25T16:23:02Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Slave Send not working as expected</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/I2C-Slave-Send-not-working-as-expected/m-p/334188#M718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a look at the I2C_LDD component user guide, it might be helpful.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this information can help you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Adrian Sanchez Cano&lt;BR /&gt;Technical Support Engineer&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2015 16:30:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/I2C-Slave-Send-not-working-as-expected/m-p/334188#M718</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2015-02-25T16:30:49Z</dc:date>
    </item>
  </channel>
</rss>