<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Program upper bank in flash in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-upper-bank-in-flash/m-p/545788#M7037</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeff&lt;/P&gt;&lt;P&gt;1) D you want put all of the&amp;nbsp; code start from 0x80000 ? If yes, you can change the linker file :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21678iB18B86F145B6E954/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If only some data , you can use the relocate function :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-104433"&gt;Relocating Code and Data Using the KDS GCC Linker File for Kinetis&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) I have not used the Xilinx SDK, maybe about the question of Xilinx, you can&lt;/P&gt;&lt;P&gt;get help form the Xilinx support .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Jul 2016 03:22:18 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2016-07-29T03:22:18Z</dc:date>
    <item>
      <title>Program upper bank in flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-upper-bank-in-flash/m-p/545785#M7034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Has anyone tried to use the Kinetis "Flash Configurations" lightning bolt menu to program the application elf file or binary image to the UPPER bank of the flash?&amp;nbsp; I think my upper bank starts at address 0x80000.&amp;nbsp; I tried entering 80000 in the offset and I did not get the results I expected.&amp;nbsp; If I leave the symbol offset and executable offset blank, the LOWER bank of the flash gets programmed correctly.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;I know in the Xilinx SDK flash utility, I need to use a binary as opposed to an ELF and specifying a flash offset will work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 19:16:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-upper-bank-in-flash/m-p/545785#M7034</guid>
      <dc:creator>jeffwood</dc:creator>
      <dc:date>2016-07-27T19:16:09Z</dc:date>
    </item>
    <item>
      <title>Re: Program upper bank in flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-upper-bank-in-flash/m-p/545786#M7035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeff,&lt;/P&gt;&lt;P&gt;Do you use KDS IDE , and kinetis chips ?&lt;/P&gt;&lt;P&gt;Have you change the linker file to start from the address 0x80000 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 02:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-upper-bank-in-flash/m-p/545786#M7035</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-07-28T02:33:45Z</dc:date>
    </item>
    <item>
      <title>Re: Program upper bank in flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-upper-bank-in-flash/m-p/545787#M7036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes KDS IDE and freescale K64F MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did not try changing the linker file.&amp;nbsp; Does that imply that the application ELF needs to be rebuilt in order to get the programmer to place the code at 0x80000?&amp;nbsp; Do you know where the linker file is accessed/edited and where the start address field would be?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You would think if I specified the binary instead of the ELF in the IDE programming utility, that I'd be able to program the flash at any offset.&amp;nbsp; Maybe that functionality is not supported (as it is in Xilinx SDK)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 13:49:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-upper-bank-in-flash/m-p/545787#M7036</guid>
      <dc:creator>jeffwood</dc:creator>
      <dc:date>2016-07-28T13:49:32Z</dc:date>
    </item>
    <item>
      <title>Re: Program upper bank in flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-upper-bank-in-flash/m-p/545788#M7037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeff&lt;/P&gt;&lt;P&gt;1) D you want put all of the&amp;nbsp; code start from 0x80000 ? If yes, you can change the linker file :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21678iB18B86F145B6E954/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If only some data , you can use the relocate function :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-104433"&gt;Relocating Code and Data Using the KDS GCC Linker File for Kinetis&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) I have not used the Xilinx SDK, maybe about the question of Xilinx, you can&lt;/P&gt;&lt;P&gt;get help form the Xilinx support .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jul 2016 03:22:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-upper-bank-in-flash/m-p/545788#M7037</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-07-29T03:22:18Z</dc:date>
    </item>
    <item>
      <title>Re: Program upper bank in flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-upper-bank-in-flash/m-p/545789#M7038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Alice,&lt;/P&gt;&lt;P&gt;I will give this a try!&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Aug 2016 14:51:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Program-upper-bank-in-flash/m-p/545789#M7038</guid>
      <dc:creator>jeffwood</dc:creator>
      <dc:date>2016-08-01T14:51:00Z</dc:date>
    </item>
  </channel>
</rss>