<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Saving and Rebuilding Working Set will  in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Saving-and-Rebuilding-Working-Set-will/m-p/544444#M7031</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello stephen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1&amp;gt; Yes ,In KDS,&amp;nbsp; open one project use the "import" button .&lt;/P&gt;&lt;P&gt;2&amp;gt; About your this question , could you please describe it clearly ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You'd better show your steps one by one , then&amp;nbsp; tell me at which step have error .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:13:47 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2016-06-16T02:13:47Z</dc:date>
    <item>
      <title>Saving and Rebuilding Working Set will</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Saving-and-Rebuilding-Working-Set-will/m-p/544443#M7030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have 2 questions:&amp;nbsp; &lt;/P&gt;&lt;P&gt;1) Best practices:&amp;nbsp; When you create a new KDS project and then save it and close it and remove it from the project pane, how do you reopen it?&amp;nbsp; The&amp;nbsp; Project -&amp;gt; Open Project is grayed out and will not browse. The only way I've figured out how to open a project is to Import it.&amp;nbsp; But that only works if there is a WorkingSet file which is not created by default.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) Creating a Working Set?&amp;nbsp;&amp;nbsp; I've figured out that I need to export to a Working Set to a file in the project director (which is a catch22 because there is no way to create the file if it doesn't exist).&amp;nbsp; So, I've created a kds directory and "touched" a file to create a wsd file.&amp;nbsp; Then I can export wsd settings into it.&amp;nbsp;&amp;nbsp;&amp;nbsp; There doesn't seem to be&amp;nbsp; away to "CREATE" a working set when you export unless I use my method above and create an empty file initially.&amp;nbsp;&amp;nbsp; Is this a bug in the KDS code?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:33:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Saving-and-Rebuilding-Working-Set-will/m-p/544443#M7030</guid>
      <dc:creator>aerodame</dc:creator>
      <dc:date>2016-06-16T00:33:20Z</dc:date>
    </item>
    <item>
      <title>Re: Saving and Rebuilding Working Set will</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Saving-and-Rebuilding-Working-Set-will/m-p/544444#M7031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello stephen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1&amp;gt; Yes ,In KDS,&amp;nbsp; open one project use the "import" button .&lt;/P&gt;&lt;P&gt;2&amp;gt; About your this question , could you please describe it clearly ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You'd better show your steps one by one , then&amp;nbsp; tell me at which step have error .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:13:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Saving-and-Rebuilding-Working-Set-will/m-p/544444#M7031</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-06-16T02:13:47Z</dc:date>
    </item>
    <item>
      <title>Re: Saving and Rebuilding Working Set will</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Saving-and-Rebuilding-Working-Set-will/m-p/544445#M7032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stephen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;use File &amp;gt; Import &amp;gt; General &amp;gt; Existing Projects into Workspace&lt;/P&gt;&lt;P&gt;Select root directory: select your workspace&lt;/P&gt;&lt;P&gt;You should see your project there, if you did not remove sources. I have just tried in KDS 3.2 and it worked well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 13:37:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Saving-and-Rebuilding-Working-Set-will/m-p/544445#M7032</guid>
      <dc:creator>MarekTrmac</dc:creator>
      <dc:date>2016-06-16T13:37:23Z</dc:date>
    </item>
    <item>
      <title>Re: Saving and Rebuilding Working Set will</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Saving-and-Rebuilding-Working-Set-will/m-p/544446#M7033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, that worked.&amp;nbsp; I was trying to import from the Project of Projects method.&amp;nbsp;&amp;nbsp;&amp;nbsp; The problem still exists on being able to export a Working Set file if it doesn't exist already.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I start from scratch and create a Kinetis 2.0 project, then check to make sure that it builds and I can run the debugger on the FRDM-K22F boards that I have.&amp;nbsp; Then I create a Working Set by some name related to this project.&amp;nbsp; (which is a bit misleading because it doesn't store that with the project in that instant.&amp;nbsp; Then I thought the right thing to do was to export to create (store) the projectname.wsd file.&amp;nbsp; When the export can't find a file by that name it won't create one... (this is the confusing part for me -- why?)... SO I just coerce it to store a file, by going to my mac terminal and "touching" a wsd file in a folder (also doesn't exist) called kds.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I can save(export) to that wsd and all is well.&amp;nbsp; I can then save this all to GIT, check out to other machines and use import to pull the whole project in by its working set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I now see that I can save and restore projects by the GENERAL option.&amp;nbsp; So, maybe I'm trying too hard by using the WSD.&amp;nbsp;&amp;nbsp; But that is the design pattern I saw in all the example files so I thought that was the way to go.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 00:11:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Saving-and-Rebuilding-Working-Set-will/m-p/544446#M7033</guid>
      <dc:creator>aerodame</dc:creator>
      <dc:date>2016-06-17T00:11:07Z</dc:date>
    </item>
  </channel>
</rss>