<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: Usage of function RxCallback for fsl_uart component</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Usage-of-function-RxCallback-for-fsl-uart-component/m-p/513647#M6769</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;see this thread&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/395820"&gt;How can I use RxCallback for fsl_uart component&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Jun 2016 05:58:40 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2016-06-03T05:58:40Z</dc:date>
    <item>
      <title>Usage of function RxCallback for fsl_uart component</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Usage-of-function-RxCallback-for-fsl-uart-component/m-p/513646#M6768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm new in KDS and Kinetis FRDM, but I wanna use a interruption for receive data from UART.&lt;/P&gt;&lt;P&gt;I'm using fsl_uart component whit the Rx configuration in the image.&lt;/P&gt;&lt;P&gt;Can someone tell me, how and when is the UART_RxCallback(uint32_t instance, void * uartState) works?&lt;/P&gt;&lt;P&gt;or if I can use it as interrupt for mi program?.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121709iC171F49A29735F9F/image-size/large?v=v2&amp;amp;px=999" title="152850_152850.png" alt="152850_152850.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59155iD9B2DC0B26953D78/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jun 2016 23:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Usage-of-function-RxCallback-for-fsl-uart-component/m-p/513646#M6768</guid>
      <dc:creator>sergiosaucedo</dc:creator>
      <dc:date>2016-06-02T23:03:20Z</dc:date>
    </item>
    <item>
      <title>Re: Usage of function RxCallback for fsl_uart component</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Usage-of-function-RxCallback-for-fsl-uart-component/m-p/513647#M6769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;see this thread&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/395820"&gt;How can I use RxCallback for fsl_uart component&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2016 05:58:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Usage-of-function-RxCallback-for-fsl-uart-component/m-p/513647#M6769</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-06-03T05:58:40Z</dc:date>
    </item>
  </channel>
</rss>