<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: MK24FN256xxx12 missing in processor selection while creating a new Kinetis project</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/MK24FN256xxx12-missing-in-processor-selection-while-creating-a/m-p/512346#M6725</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rupesh,&lt;/P&gt;&lt;P&gt;Please refer to this thread to download and install the KSDK1.3 for MK24FN256xxx12:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329662"&gt;Using Kinetis Design Studio v3.x with Kinetis SDK v2.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56936i1158C408DD7E94E3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;then when you create project , you can see this option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 May 2016 01:35:03 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2016-05-11T01:35:03Z</dc:date>
    <item>
      <title>MK24FN256xxx12 missing in processor selection while creating a new Kinetis project</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/MK24FN256xxx12-missing-in-processor-selection-while-creating-a/m-p/512345#M6724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello, I need to include processor MK24FN256xxx12 for my project and I couldn't find it under the processors in devices. The only processor I was able to use was MK24Fn1M0xx12 but when I tried to load my code in internal flash, I get errors. However I was able to run the code if I download it in RAM. I assume this has to do with having different variant of the board. &lt;/P&gt;&lt;P&gt;How can I add MK24FN256xxx12 in the project?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 May 2016 14:23:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/MK24FN256xxx12-missing-in-processor-selection-while-creating-a/m-p/512345#M6724</guid>
      <dc:creator>rupeshgajurel</dc:creator>
      <dc:date>2016-05-10T14:23:35Z</dc:date>
    </item>
    <item>
      <title>Re: MK24FN256xxx12 missing in processor selection while creating a new Kinetis project</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/MK24FN256xxx12-missing-in-processor-selection-while-creating-a/m-p/512346#M6725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rupesh,&lt;/P&gt;&lt;P&gt;Please refer to this thread to download and install the KSDK1.3 for MK24FN256xxx12:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329662"&gt;Using Kinetis Design Studio v3.x with Kinetis SDK v2.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56936i1158C408DD7E94E3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;then when you create project , you can see this option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 May 2016 01:35:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/MK24FN256xxx12-missing-in-processor-selection-while-creating-a/m-p/512346#M6725</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-05-11T01:35:03Z</dc:date>
    </item>
  </channel>
</rss>