<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Parallel Build Prevents Pre/Post Build Commands in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Parallel-Build-Prevents-Pre-Post-Build-Commands/m-p/508917#M6589</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;... At lease it works for some. I guess I will create a test project.&lt;/P&gt;&lt;P&gt;And the link does not apply, i think.&lt;/P&gt;&lt;P&gt;It is very odd, I have two machines same setup same issue. and I am trying to compile the MQX psp and bsp for my board and the pre/post commands only run with parallel buildi off.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Dec 2015 21:24:54 GMT</pubDate>
    <dc:creator>leifzars</dc:creator>
    <dc:date>2015-12-29T21:24:54Z</dc:date>
    <item>
      <title>Parallel Build Prevents Pre/Post Build Commands</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Parallel-Build-Prevents-Pre-Post-Build-Commands/m-p/508915#M6587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pre and Post build commands only run when Parallel build is disabled, when enabled they do not run.&lt;/P&gt;&lt;P&gt;Is this a bug?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Windows 7 KDS 3&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Dec 2015 22:25:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Parallel-Build-Prevents-Pre-Post-Build-Commands/m-p/508915#M6587</guid>
      <dc:creator>leifzars</dc:creator>
      <dc:date>2015-12-28T22:25:17Z</dc:date>
    </item>
    <item>
      <title>Re: Parallel Build Prevents Pre/Post Build Commands</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Parallel-Build-Prevents-Pre-Post-Build-Commands/m-p/508916#M6588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leif,&lt;/P&gt;&lt;P&gt;pre- and post-build steps work for me with parallel build enabled (using Win7 too). But there is a known issue in case you have custom per-file or per-folder options set, see &lt;A href="http://mcuoneclipse.com/2013/06/12/traps-and-pitfalls-no-hexbins19-file-created-with-gnu/" title="http://mcuoneclipse.com/2013/06/12/traps-and-pitfalls-no-hexbins19-file-created-with-gnu/"&gt;Traps and Pitfalls: No Hex/Bin/S19 File Created with GNU? | MCU on Eclipse&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;This is my setup:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31697i5D452AAD0536FB65/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Dec 2015 07:26:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Parallel-Build-Prevents-Pre-Post-Build-Commands/m-p/508916#M6588</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-12-29T07:26:06Z</dc:date>
    </item>
    <item>
      <title>Re: Parallel Build Prevents Pre/Post Build Commands</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Parallel-Build-Prevents-Pre-Post-Build-Commands/m-p/508917#M6589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;... At lease it works for some. I guess I will create a test project.&lt;/P&gt;&lt;P&gt;And the link does not apply, i think.&lt;/P&gt;&lt;P&gt;It is very odd, I have two machines same setup same issue. and I am trying to compile the MQX psp and bsp for my board and the pre/post commands only run with parallel buildi off.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Dec 2015 21:24:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Parallel-Build-Prevents-Pre-Post-Build-Commands/m-p/508917#M6589</guid>
      <dc:creator>leifzars</dc:creator>
      <dc:date>2015-12-29T21:24:54Z</dc:date>
    </item>
  </channel>
</rss>