<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Code example KV5x ADC in differential mode please in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Code-example-KV5x-ADC-in-differential-mode-please/m-p/503795#M6375</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Many thanks for the example code :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Apr 2016 10:44:26 GMT</pubDate>
    <dc:creator>winpennyjh</dc:creator>
    <dc:date>2016-04-19T10:44:26Z</dc:date>
    <item>
      <title>Code example KV5x ADC in differential mode please</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Code-example-KV5x-ADC-in-differential-mode-please/m-p/503793#M6373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I need a code example of using the KV5x ADC in differential mode please.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Apr 2016 11:55:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Code-example-KV5x-ADC-in-differential-mode-please/m-p/503793#M6373</guid>
      <dc:creator>winpennyjh</dc:creator>
      <dc:date>2016-04-14T11:55:11Z</dc:date>
    </item>
    <item>
      <title>Re: Code example KV5x ADC in differential mode please</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Code-example-KV5x-ADC-in-differential-mode-please/m-p/503794#M6374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Julian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis KV5x series has 2 different ADC modules: 16-bit SAR ADC and 12-bit High Speed ADC (5MSPS).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For 16-bit SAR, this is the same module that is located in some Kinetis families, such as Kinetis 120MHz, with some little differences that are shown here: &lt;A href="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN5117.pdf?fpsp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN5117.pdf?fpsp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;http://cache.nxp.com/files/microcontrollers/doc/app_note/AN5117.pdf?fpsp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCA…&lt;/A&gt; . These differences are&amp;nbsp; basically only one ADC instance, remove PGA module and other little differences in clock selection sources and trigger selection. You can use the Kinetis Migration Guide: K10 - 120 MHz to KV5x guide to migrate attached sample code that was created for K10_120MHz target. Sample code is reading ADC0_DP0 and ADC0_DM0 inputs in its basic configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For HSADC module, There are no example codes for now (remember that KV5x part is still under preproduction stage). As soon as it gets ready for production, we can create sample codes for this module. Also, Kinetis SDK v2.0 is planned to support Kinetis V series family in mid July: &lt;A href="https://community.nxp.com/docs/DOC-329783"&gt;Introducing Kinetis SDK v2.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For now, I hope this basic example code for 16-bit SAR configured in differential mode can be used as reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Isaac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Apr 2016 17:01:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Code-example-KV5x-ADC-in-differential-mode-please/m-p/503794#M6374</guid>
      <dc:creator>isaacavila</dc:creator>
      <dc:date>2016-04-18T17:01:48Z</dc:date>
    </item>
    <item>
      <title>Re: Code example KV5x ADC in differential mode please</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Code-example-KV5x-ADC-in-differential-mode-please/m-p/503795#M6375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Many thanks for the example code :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Apr 2016 10:44:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Code-example-KV5x-ADC-in-differential-mode-please/m-p/503795#M6375</guid>
      <dc:creator>winpennyjh</dc:creator>
      <dc:date>2016-04-19T10:44:26Z</dc:date>
    </item>
  </channel>
</rss>