<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 kboot import</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/kboot-import/m-p/494389#M6042</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Setup is KDS on linux 64 bit,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;trying to set up a kboot project.&lt;/P&gt;&lt;P&gt;If I set up a new workspace and import with copy of the desired target, it sets it up but does not copy all the source files , only I2C driver??? and complains about paths being wrong, but does make an elf file..&lt;/P&gt;&lt;P&gt;If I switch to the bootloader folder as the workspace and select a project, it trashes stuff.&lt;/P&gt;&lt;P&gt;There is no way to directly open the workspace under \kds folder.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so WHAT is the EXACT procedure for setting up a bootloader project that does not modify the original sources...&lt;/P&gt;&lt;P&gt;Reference manual only shows an IAR setup..which I don't care about...&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 May 2016 17:16:15 GMT</pubDate>
    <dc:creator>kennethtait</dc:creator>
    <dc:date>2016-05-23T17:16:15Z</dc:date>
    <item>
      <title>kboot import</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/kboot-import/m-p/494389#M6042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Setup is KDS on linux 64 bit,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;trying to set up a kboot project.&lt;/P&gt;&lt;P&gt;If I set up a new workspace and import with copy of the desired target, it sets it up but does not copy all the source files , only I2C driver??? and complains about paths being wrong, but does make an elf file..&lt;/P&gt;&lt;P&gt;If I switch to the bootloader folder as the workspace and select a project, it trashes stuff.&lt;/P&gt;&lt;P&gt;There is no way to directly open the workspace under \kds folder.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so WHAT is the EXACT procedure for setting up a bootloader project that does not modify the original sources...&lt;/P&gt;&lt;P&gt;Reference manual only shows an IAR setup..which I don't care about...&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 May 2016 17:16:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/kboot-import/m-p/494389#M6042</guid>
      <dc:creator>kennethtait</dc:creator>
      <dc:date>2016-05-23T17:16:15Z</dc:date>
    </item>
    <item>
      <title>Re: kboot import</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/kboot-import/m-p/494390#M6043</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kenneth,&lt;/P&gt;&lt;P&gt;Which version of KBOOT do you used ?&lt;/P&gt;&lt;P&gt;I recommend you use the latest version KBOOT v2.0 ,&amp;nbsp; KDSv3.2 .&lt;/P&gt;&lt;P&gt;And when i used it on&amp;nbsp; Wind7, the bootloader project on be import well .'&lt;/P&gt;&lt;P&gt;While when you use it , if the image outside of the memory size , there is two method to fix,you can refer to this DOC: &lt;A href="https://community.nxp.com/docs/DOC-331375"&gt;Using KBOOT v2 on KDS in Debug Mode&lt;/A&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 May 2016 02:06:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/kboot-import/m-p/494390#M6043</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-05-24T02:06:08Z</dc:date>
    </item>
    <item>
      <title>Re: kboot import</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/kboot-import/m-p/494391#M6044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the 2.0 version. the problems here are many...&lt;/P&gt;&lt;P&gt;Overall, the bootloader itself is pretty good, addresses most everything &lt;/P&gt;&lt;P&gt;needed, except in my case...&lt;/P&gt;&lt;P&gt;The Docs only address an IAR port, which is a serious omission since we &lt;/P&gt;&lt;P&gt;are being told Kinetis is the future...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First of all, there are no header,linker or startup files for the part &lt;/P&gt;&lt;P&gt;I'm using, MK22FN1m0, so using the 512k which should be close.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Second, if you import the bootloader, what you get are virtual links to &lt;/P&gt;&lt;P&gt;all the files. It compiles, you can change minor things and get a build, &lt;/P&gt;&lt;P&gt;but if you try and generate any new files to link in, such as needing to &lt;/P&gt;&lt;P&gt;run a simple display, this fails. You can't make any new files, since &lt;/P&gt;&lt;P&gt;essentially there is NO main folder. Importing with copy fails too. &lt;/P&gt;&lt;P&gt;There should be no reason for this.... Having to use the the actual &lt;/P&gt;&lt;P&gt;disti makes it very difficult to archive projects correctly....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;trying to copy over all the relevant pieces into a new project should be &lt;/P&gt;&lt;P&gt;the cleanest way to go, but it won't build since the file links are broken.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All pathways are blocked here...Why can't this this just be a simple set &lt;/P&gt;&lt;P&gt;of files that customers can modify. If we screw it up it's our &lt;/P&gt;&lt;P&gt;issue..not yours.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I haven't used Eclipse in some time and I'm now remembering what a &lt;/P&gt;&lt;P&gt;crappy IDE it really is :smileysad:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 May 2016 16:51:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/kboot-import/m-p/494391#M6044</guid>
      <dc:creator>kennethtait</dc:creator>
      <dc:date>2016-05-24T16:51:40Z</dc:date>
    </item>
    <item>
      <title>Re: kboot import</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/kboot-import/m-p/494392#M6045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kenneth,&lt;/P&gt;&lt;P&gt;Oh , you want porting the bootlaoder to MK22fn1m0 chip .&lt;/P&gt;&lt;P&gt;If you think it is hard to port the KBOOT v2.0 , i&amp;nbsp; recommend you another simple bootlaoder.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-328365"&gt;Kinetis Bootloader to Update Multiple Devices in a Network for Cortex-M4&lt;/A&gt; &lt;/P&gt;&lt;P&gt;This is simple of KBOOT, it is for FRDM-K22(the chip is k22fn512), it include KDS v3.0 version , keil, IAR.&lt;/P&gt;&lt;P&gt;And&amp;nbsp; thay all of independent files , not have the virtual file .&lt;/P&gt;&lt;P&gt;Also there is the Reference manual to introduce it , the process is the same as KBOOT.&lt;/P&gt;&lt;P&gt;I think after you check , you can porting it to K22FN1M0 chip , only need change some flash address and size place.&lt;/P&gt;&lt;P&gt;And i know clearly about this bootlaoder , so when you porting , if there is some problem you can contact me without&lt;/P&gt;&lt;P&gt;any hesitate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 May 2016 03:04:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/kboot-import/m-p/494392#M6045</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-05-25T03:04:15Z</dc:date>
    </item>
    <item>
      <title>Re: kboot import</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/kboot-import/m-p/494393#M6046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Alice!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was not aware of this and I will definitely look it over. We only need &lt;/P&gt;&lt;P&gt;a simple bootloader for this project that does not need all the KBOOT &lt;/P&gt;&lt;P&gt;features&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 May 2016 14:46:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/kboot-import/m-p/494393#M6046</guid>
      <dc:creator>kennethtait</dc:creator>
      <dc:date>2016-05-25T14:46:49Z</dc:date>
    </item>
    <item>
      <title>Re: kboot import</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/kboot-import/m-p/494394#M6047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ken,&lt;/P&gt;&lt;P&gt;Yes, it is simple than KBOOT, it only use the UART to update .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 May 2016 01:33:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/kboot-import/m-p/494394#M6047</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-05-26T01:33:10Z</dc:date>
    </item>
  </channel>
</rss>