<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックUnresolved inclusion warnings</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Unresolved-inclusion-warnings/m-p/490019#M5884</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Something a little strange I'm seeing in KDS.&amp;nbsp; Seems to be an Eclipse issue, but it's not making sense.&amp;nbsp; I have multiple source files in the project.&amp;nbsp; There's a separate project in the workspace that includes several header files.&amp;nbsp; I have the top level project defined to use the includes directory I've defined, and I've used the path "${ProjDirPath}/../KELibs/Includes".&amp;nbsp; If I look under the C/C++ general properties, I see it is resolving the path properly.&amp;nbsp; Here's what doesn't makes sense.&amp;nbsp; Some of these source files in the top level project will show several warnings about unresolved inclusions, and show syntax errors as a result.&amp;nbsp; However, other source files at the same level in the project include the exact same files, and have no warnings.&amp;nbsp; Everything builds and compiles fine, I just don't understand why all these warnings are showing up for certain files.&amp;nbsp; If I look at the properties for the files with the warnings, their include paths are correct.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Feb 2016 14:47:56 GMT</pubDate>
    <dc:creator>davidsherman</dc:creator>
    <dc:date>2016-02-04T14:47:56Z</dc:date>
    <item>
      <title>Unresolved inclusion warnings</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Unresolved-inclusion-warnings/m-p/490019#M5884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Something a little strange I'm seeing in KDS.&amp;nbsp; Seems to be an Eclipse issue, but it's not making sense.&amp;nbsp; I have multiple source files in the project.&amp;nbsp; There's a separate project in the workspace that includes several header files.&amp;nbsp; I have the top level project defined to use the includes directory I've defined, and I've used the path "${ProjDirPath}/../KELibs/Includes".&amp;nbsp; If I look under the C/C++ general properties, I see it is resolving the path properly.&amp;nbsp; Here's what doesn't makes sense.&amp;nbsp; Some of these source files in the top level project will show several warnings about unresolved inclusions, and show syntax errors as a result.&amp;nbsp; However, other source files at the same level in the project include the exact same files, and have no warnings.&amp;nbsp; Everything builds and compiles fine, I just don't understand why all these warnings are showing up for certain files.&amp;nbsp; If I look at the properties for the files with the warnings, their include paths are correct.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2016 14:47:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Unresolved-inclusion-warnings/m-p/490019#M5884</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2016-02-04T14:47:56Z</dc:date>
    </item>
    <item>
      <title>Re: Unresolved inclusion warnings</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Unresolved-inclusion-warnings/m-p/490020#M5885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;Eclipse is using the 'Index' and 'Indexer' to parse all the files in the editor (in the background) and builds up a data base.&lt;/P&gt;&lt;P&gt;It could be that this data base is not correct any more. See &lt;A href="http://mcuoneclipse.com/2012/03/20/fixing-the-eclipse-index/" title="http://mcuoneclipse.com/2012/03/20/fixing-the-eclipse-index/"&gt;Fixing the Eclipse Index | MCU on Eclipse&lt;/A&gt;&amp;nbsp; for how to fix it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2016 18:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Unresolved-inclusion-warnings/m-p/490020#M5885</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-02-04T18:33:40Z</dc:date>
    </item>
    <item>
      <title>Re: Unresolved inclusion warnings</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Unresolved-inclusion-warnings/m-p/490021#M5886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Erich, I'll take a look at that.&amp;nbsp; I can't tell if it fixed the specific problem, because it seems to have corrected itself.&amp;nbsp; Good to know, though, thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2016 14:33:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Unresolved-inclusion-warnings/m-p/490021#M5886</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2016-02-05T14:33:38Z</dc:date>
    </item>
  </channel>
</rss>