<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K64F Clock Speed And Delay in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/K64F-Clock-Speed-And-Delay/m-p/489720#M5869</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dogus,&lt;/P&gt;&lt;P&gt;There is no bare board demo delay function .&lt;/P&gt;&lt;P&gt;- About the clock , you can first read the CLOCK chapter of the Reference manual ,&lt;/P&gt;&lt;P&gt;then you can only create one simple project on KDS, then you can see the different clock mode&lt;/P&gt;&lt;P&gt;about how to configure the related registers :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56307i90671718C17A622C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;- About the delay function , you can configure the PIT timer by your self , also i think the simple&lt;/P&gt;&lt;P&gt;method is you create one PE project, then configure the&amp;nbsp; interrupt :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56360iFFAF16CBEB9B722B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Apr 2016 07:35:35 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2016-04-29T07:35:35Z</dc:date>
    <item>
      <title>K64F Clock Speed And Delay</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/K64F-Clock-Speed-And-Delay/m-p/489719#M5868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello people, recently i bought a K64F Board and i am kind of new to embedded programming scene , can somebody point me to a direction where i can learn to set which oscillator to use to set the clock speed then write a simple ms delay function. Thanks a lot &lt;SPAN aria-label="Happy" class="emoticon_happy emoticon-inline" style="height:16px;width:16px;"&gt;&lt;/SPAN&gt; (I am using KDS and avoiding to use PE and other similar programs to learn from the scratch)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2016 06:36:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/K64F-Clock-Speed-And-Delay/m-p/489719#M5868</guid>
      <dc:creator>dogusural</dc:creator>
      <dc:date>2016-04-29T06:36:35Z</dc:date>
    </item>
    <item>
      <title>Re: K64F Clock Speed And Delay</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/K64F-Clock-Speed-And-Delay/m-p/489720#M5869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dogus,&lt;/P&gt;&lt;P&gt;There is no bare board demo delay function .&lt;/P&gt;&lt;P&gt;- About the clock , you can first read the CLOCK chapter of the Reference manual ,&lt;/P&gt;&lt;P&gt;then you can only create one simple project on KDS, then you can see the different clock mode&lt;/P&gt;&lt;P&gt;about how to configure the related registers :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56307i90671718C17A622C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;- About the delay function , you can configure the PIT timer by your self , also i think the simple&lt;/P&gt;&lt;P&gt;method is you create one PE project, then configure the&amp;nbsp; interrupt :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56360iFFAF16CBEB9B722B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2016 07:35:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/K64F-Clock-Speed-And-Delay/m-p/489720#M5869</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-04-29T07:35:35Z</dc:date>
    </item>
  </channel>
</rss>