<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: TWR-K65F180M Debug Config Setup</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K65F180M-Debug-Config-Setup/m-p/483444#M5589</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jake,&lt;/P&gt;&lt;P&gt;Did you update the TWR-K65F180M debugging firmware to support Pemicro?&lt;/P&gt;&lt;P&gt;If not the ZIP is attached.&amp;nbsp; Unplug the USB debug cable, hold reset button down, plug-in USB debug cable, and system should enumerate as a MSD.&lt;/P&gt;&lt;P&gt;Then drag-n-drop the *.bin file to the BOOTLOADER disk.&amp;nbsp; After a few seconds new firmware should be loaded.&amp;nbsp; Unplug and re-plug and you should have the Pemico OpenSDA interface enumerated.&lt;/P&gt;&lt;P&gt;Then back in debugger you should see it.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;PS ignore the name of the ZIP and file...it really does work with TWR-K65F180M.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Feb 2016 16:03:52 GMT</pubDate>
    <dc:creator>DavidS</dc:creator>
    <dc:date>2016-02-02T16:03:52Z</dc:date>
    <item>
      <title>TWR-K65F180M Debug Config Setup</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K65F180M-Debug-Config-Setup/m-p/483443#M5588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have just started using the TWR-K65F180M and am running through setting up the debug configurations as laid out in the getting started with KSDK videos.&amp;nbsp; The issue I am having is when setting up the PEMicro Interface Port I have no port options(see picture below). Examples I have seen "USB1 - OpenSDA" example is available and selected. How do I achieve this?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="135623_135623.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121036i5EE15BD303587B64/image-size/large?v=v2&amp;amp;px=999" role="button" title="135623_135623.png" alt="135623_135623.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52261iB39F516046A38710/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Feb 2016 13:42:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K65F180M-Debug-Config-Setup/m-p/483443#M5588</guid>
      <dc:creator>henninjw</dc:creator>
      <dc:date>2016-02-02T13:42:56Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K65F180M Debug Config Setup</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K65F180M-Debug-Config-Setup/m-p/483444#M5589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jake,&lt;/P&gt;&lt;P&gt;Did you update the TWR-K65F180M debugging firmware to support Pemicro?&lt;/P&gt;&lt;P&gt;If not the ZIP is attached.&amp;nbsp; Unplug the USB debug cable, hold reset button down, plug-in USB debug cable, and system should enumerate as a MSD.&lt;/P&gt;&lt;P&gt;Then drag-n-drop the *.bin file to the BOOTLOADER disk.&amp;nbsp; After a few seconds new firmware should be loaded.&amp;nbsp; Unplug and re-plug and you should have the Pemico OpenSDA interface enumerated.&lt;/P&gt;&lt;P&gt;Then back in debugger you should see it.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;PS ignore the name of the ZIP and file...it really does work with TWR-K65F180M.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Feb 2016 16:03:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K65F180M-Debug-Config-Setup/m-p/483444#M5589</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2016-02-02T16:03:52Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K65F180M Debug Config Setup</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K65F180M-Debug-Config-Setup/m-p/483445#M5590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Feb 2016 16:19:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K65F180M-Debug-Config-Setup/m-p/483445#M5590</guid>
      <dc:creator>henninjw</dc:creator>
      <dc:date>2016-02-02T16:19:15Z</dc:date>
    </item>
  </channel>
</rss>