<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: Can't Create Processor Expert Project for MK24FN1M0VLL12</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Can-t-Create-Processor-Expert-Project-for-MK24FN1M0VLL12/m-p/482595#M5536</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was finally able to get it working with the KSDK V 1.3 I created for the micro I am using and the New KSDK 1.X&amp;nbsp; or PE Project command.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Apr 2016 17:01:11 GMT</pubDate>
    <dc:creator>dmushow</dc:creator>
    <dc:date>2016-04-28T17:01:11Z</dc:date>
    <item>
      <title>Can't Create Processor Expert Project for MK24FN1M0VLL12</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Can-t-Create-Processor-Expert-Project-for-MK24FN1M0VLL12/m-p/482593#M5534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have made several attempts to create a processor expert project for the MK24FN1M0VLL12.&amp;nbsp; Every way I have tried results in the MK24FN1M0VLL12 being excluded from the drop down menu of processors available.&amp;nbsp; If I delete the processor from the project and attempt to add the exact processor I am interested in from the component library, the add feature fails to add anything to the project.&amp;nbsp; Below are pictures of the installed options and the project with the drop down list excluding the VLL12 processor.&amp;nbsp; Am I missing something? do I need to uninstall KDS and reinstall it?&amp;nbsp; Any help on the matter is greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121488iF5A2EE0625374E02/image-size/large?v=v2&amp;amp;px=999" title="146924_146924.png" alt="146924_146924.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36375i251C9CAC2C3A06D5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121489i7455626ACB70A419/image-size/large?v=v2&amp;amp;px=999" title="146925_146925.png" alt="146925_146925.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36423i33CDA2DC7D33FB31/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 17:00:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Can-t-Create-Processor-Expert-Project-for-MK24FN1M0VLL12/m-p/482593#M5534</guid>
      <dc:creator>dmushow</dc:creator>
      <dc:date>2016-04-27T17:00:44Z</dc:date>
    </item>
    <item>
      <title>Re: Can't Create Processor Expert Project for MK24FN1M0VLL12</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Can-t-Create-Processor-Expert-Project-for-MK24FN1M0VLL12/m-p/482594#M5535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;Can you use the KSDK+PE? &lt;/P&gt;&lt;P&gt;In the KSDK+PE project, there is the chip of MK24FN1M0VLL12:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54310iC174C52B2929C39F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I use KSDK1.3, i see you install KSDK1.2, i think the ksdk1.2 also have , if it not have , you can insatll&lt;/P&gt;&lt;P&gt;the version of KSDK1.3 .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 01:45:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Can-t-Create-Processor-Expert-Project-for-MK24FN1M0VLL12/m-p/482594#M5535</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-04-28T01:45:04Z</dc:date>
    </item>
    <item>
      <title>Re: Can't Create Processor Expert Project for MK24FN1M0VLL12</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Can-t-Create-Processor-Expert-Project-for-MK24FN1M0VLL12/m-p/482595#M5536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was finally able to get it working with the KSDK V 1.3 I created for the micro I am using and the New KSDK 1.X&amp;nbsp; or PE Project command.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 17:01:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Can-t-Create-Processor-Expert-Project-for-MK24FN1M0VLL12/m-p/482595#M5536</guid>
      <dc:creator>dmushow</dc:creator>
      <dc:date>2016-04-28T17:01:11Z</dc:date>
    </item>
  </channel>
</rss>