<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: debug with 2 emulators in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/debug-with-2-emulators/m-p/481734#M5480</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich if it can help I tried with KDS 3.1.0 and CW 10.6 in the same PC at the same moment and I can debug together without problems.&lt;/P&gt;&lt;P&gt;Both have the same kind of emulator (Multilink Universal). Of course each one on a different USB port.....&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Salvatore&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jan 2016 10:07:41 GMT</pubDate>
    <dc:creator>Salva</dc:creator>
    <dc:date>2016-01-14T10:07:41Z</dc:date>
    <item>
      <title>debug with 2 emulators</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/debug-with-2-emulators/m-p/481731#M5477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi to all I've got this problem: how can I debug with 2 emulators ? Till I was using Codewarrior (10.6) I haven't any problem. With KDS (both 3.0.0 and now 3.1.0) it doesn't work. The message is the same (with one emulator) if you try to run again a debug session without closing the last one. The message is:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120968iB7B202A34445420E/image-size/large?v=v2&amp;amp;px=999" title="126697_126697.png" alt="126697_126697.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31262iB52B976163CC5306/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried also lunching a second istance of KDS with same behavior . &lt;/P&gt;&lt;P&gt;The problem seem to be on Multilink Universal driver&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another question: is it possible to make an hard reset to CPU (there is the 'restart' button, but it doesn't make a Hardware reset to CPU).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Actually I'm using KDS 3.1.0, K64 microcontroller, Windows 10 64 bit&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone help me ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jan 2016 09:55:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/debug-with-2-emulators/m-p/481731#M5477</guid>
      <dc:creator>Salva</dc:creator>
      <dc:date>2016-01-11T09:55:50Z</dc:date>
    </item>
    <item>
      <title>Re: debug with 2 emulators</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/debug-with-2-emulators/m-p/481732#M5478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No one has this problem ?&lt;/P&gt;&lt;P&gt;Is it possible to try some 'workaround' ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 18:16:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/debug-with-2-emulators/m-p/481732#M5478</guid>
      <dc:creator>Salva</dc:creator>
      <dc:date>2016-01-12T18:16:02Z</dc:date>
    </item>
    <item>
      <title>Re: debug with 2 emulators</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/debug-with-2-emulators/m-p/481733#M5479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did that, bascially means setting up a connection with a different port. I only need to find some spare time to document and post it :-(&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 20:43:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/debug-with-2-emulators/m-p/481733#M5479</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-01-12T20:43:15Z</dc:date>
    </item>
    <item>
      <title>Re: debug with 2 emulators</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/debug-with-2-emulators/m-p/481734#M5480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich if it can help I tried with KDS 3.1.0 and CW 10.6 in the same PC at the same moment and I can debug together without problems.&lt;/P&gt;&lt;P&gt;Both have the same kind of emulator (Multilink Universal). Of course each one on a different USB port.....&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Salvatore&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jan 2016 10:07:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/debug-with-2-emulators/m-p/481734#M5480</guid>
      <dc:creator>Salva</dc:creator>
      <dc:date>2016-01-14T10:07:41Z</dc:date>
    </item>
    <item>
      <title>Re: debug with 2 emulators</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/debug-with-2-emulators/m-p/481735#M5481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Salvatore,&lt;/P&gt;&lt;P&gt;I'm able to do this with the Segger connection (either J-Link or OpenSDA), see &lt;A href="http://mcuoneclipse.com/2016/01/23/debug-multiple-boards-with-gdb-at-the-same-time/" title="http://mcuoneclipse.com/2016/01/23/debug-multiple-boards-with-gdb-at-the-same-time/"&gt;Debug Multiple Boards with GDB at the Same Time | MCU on Eclipse&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;I have not been able to do the same with the P&amp;amp;E Multilinks. The same approach (using different TCP/IP ports) should work for the Multilinks too, but I have not seen a setting in the panel for this. When I started the P&amp;amp;E server with different ports it did not work for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jan 2016 09:31:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/debug-with-2-emulators/m-p/481735#M5481</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-01-23T09:31:48Z</dc:date>
    </item>
  </channel>
</rss>