<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: In need for a Jlink bootloader MK20DX128VFM5 project for the FRDM-K82F board</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/In-need-for-a-Jlink-bootloader-MK20DX128VFM5-project-for-the/m-p/479041#M5388</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ben,&lt;/P&gt;&lt;P&gt;Attached is ZIP with a binary and s-record file of the FRDM-K82F k20dx128 debugger firmware.&lt;/P&gt;&lt;P&gt;I used CW10.6 with Segger JLink to extract the binary/s-record.&lt;/P&gt;&lt;P&gt;I then used KDS_3.0 to create a new PE project for k20dx128 device (had to use PE to change the processor package but you actually probably do not need to do this set) with Segger JLink.&amp;nbsp; I ran the test project on the k20dx128 on the FRDM-K82F to see that it was working.&amp;nbsp; Then used the "lightning bolt" to program the s-record to the k20dx128 to get the debug bootloader working again.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Apr 2016 22:05:37 GMT</pubDate>
    <dc:creator>DavidS</dc:creator>
    <dc:date>2016-04-04T22:05:37Z</dc:date>
    <item>
      <title>In need for a Jlink bootloader MK20DX128VFM5 project for the FRDM-K82F board</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/In-need-for-a-Jlink-bootloader-MK20DX128VFM5-project-for-the/m-p/479040#M5387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just got the FRDM-K82F board Saturday. When following the video instructions on "How to get started"&amp;nbsp; found at &lt;A href="https://community.nxp.com/www.nxp.com/FRDM-K82F/startnow" target="test_blank"&gt;www.nxp.com/FRDM-K82F/startnow&lt;/A&gt;, when following the step, of pressing the reset button and plugging in the board. The bootloader directory shows up in the File Explorer, as it should. But when I moved the&lt;/P&gt;&lt;P&gt;"Jlink_OpenSDA_V2_1_2015-10-13.bin" file to the bootloader directory in the explorer window, the PC gave me an error message box saying that the file can not be found.&lt;/P&gt;&lt;P&gt;Now the FRDM board is not recognized when I plug in the USB cable with the reset button down or up. I'm guessing the bootloader is broke.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can load new projects into the board using the MK82FN256VLL15 10 processor via its 10pin-JTAG connector.&lt;/P&gt;&lt;P&gt;I also can load new projects for the MK20DX128VFM5 processors via its 10pin Jtag connector. (The SDA USB bootloader chip).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anyone has an SDA Jlink elf file, then I can reprogram the MK20DX128VFM5 through the JTAG connector.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have no knowledge of how to program a bin file using the Segger hardware debugger. I tried to do it in the debugger source tab, but no joy.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt; Ben&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Apr 2016 16:23:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/In-need-for-a-Jlink-bootloader-MK20DX128VFM5-project-for-the/m-p/479040#M5387</guid>
      <dc:creator>benmccormick</dc:creator>
      <dc:date>2016-04-04T16:23:57Z</dc:date>
    </item>
    <item>
      <title>Re: In need for a Jlink bootloader MK20DX128VFM5 project for the FRDM-K82F board</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/In-need-for-a-Jlink-bootloader-MK20DX128VFM5-project-for-the/m-p/479041#M5388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ben,&lt;/P&gt;&lt;P&gt;Attached is ZIP with a binary and s-record file of the FRDM-K82F k20dx128 debugger firmware.&lt;/P&gt;&lt;P&gt;I used CW10.6 with Segger JLink to extract the binary/s-record.&lt;/P&gt;&lt;P&gt;I then used KDS_3.0 to create a new PE project for k20dx128 device (had to use PE to change the processor package but you actually probably do not need to do this set) with Segger JLink.&amp;nbsp; I ran the test project on the k20dx128 on the FRDM-K82F to see that it was working.&amp;nbsp; Then used the "lightning bolt" to program the s-record to the k20dx128 to get the debug bootloader working again.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Apr 2016 22:05:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/In-need-for-a-Jlink-bootloader-MK20DX128VFM5-project-for-the/m-p/479041#M5388</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2016-04-04T22:05:37Z</dc:date>
    </item>
    <item>
      <title>Re: In need for a Jlink bootloader MK20DX128VFM5 project for the FRDM-K82F board</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/In-need-for-a-Jlink-bootloader-MK20DX128VFM5-project-for-the/m-p/479042#M5389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI David,&lt;/P&gt;&lt;P&gt; Thanks! That got the board back on its feet.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt; Ben&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 13:58:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/In-need-for-a-Jlink-bootloader-MK20DX128VFM5-project-for-the/m-p/479042#M5389</guid>
      <dc:creator>benmccormick</dc:creator>
      <dc:date>2016-04-05T13:58:43Z</dc:date>
    </item>
    <item>
      <title>Re: In need for a Jlink bootloader MK20DX128VFM5 project for the FRDM-K82F board</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/In-need-for-a-Jlink-bootloader-MK20DX128VFM5-project-for-the/m-p/479043#M5390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good to know.&amp;nbsp; Thanks for updating the post as I'm sure it will help others too.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 16:13:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/In-need-for-a-Jlink-bootloader-MK20DX128VFM5-project-for-the/m-p/479043#M5390</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2016-04-05T16:13:38Z</dc:date>
    </item>
  </channel>
</rss>