<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: Is OpenOCD supported now for the MacOSX</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-OpenOCD-supported-now-for-the-MacOSX/m-p/478698#M5380</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks... after a few fits and starts I finally decided to uninstall KDS and ensure that the Segger OpenSDA was installed properly by dragging the bin (JLink_OpenSDA_V2_1_2015-10-13.bin) to the bootloader folder on the Mac file system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I reinstalled KDS and tried a few example projects all is well!&amp;nbsp; I have to say it is fantastic to be able to develop on the Mac after all these years.&amp;nbsp; The FRDM-K22F and being able to just debug with a USB cable is wonderful!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 May 2016 23:16:56 GMT</pubDate>
    <dc:creator>aerodame</dc:creator>
    <dc:date>2016-05-17T23:16:56Z</dc:date>
    <item>
      <title>Is OpenOCD supported now for the MacOSX</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-OpenOCD-supported-now-for-the-MacOSX/m-p/478696#M5378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've just downloaded the latest KDSv3, installed in my Mac, but all of the older posts claim that OpenOCD is not compatible with MacOSX and FRDM-K22F.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just want to do a simple download and debug and it is enormously confusing with seemingly contradicting information out there on which driver works and what configuration files to use, etc.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do we use OpenSDA (from SEGGER) or OpenOCD (from who?)&amp;nbsp; What's been tested?&amp;nbsp; WHere are links to everything that is needed and why isn't all of this right on the home page of the FRDM-K22F?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 May 2016 19:58:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-OpenOCD-supported-now-for-the-MacOSX/m-p/478696#M5378</guid>
      <dc:creator>aerodame</dc:creator>
      <dc:date>2016-05-17T19:58:39Z</dc:date>
    </item>
    <item>
      <title>Re: Is OpenOCD supported now for the MacOSX</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-OpenOCD-supported-now-for-the-MacOSX/m-p/478697#M5379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stephen,&lt;/P&gt;&lt;P&gt;what comes with KDS V3.x for Mac OS X is Segger J-Link support. You can load the Segger J-Link firmware from Segger on the OpenSDA K20 debug chip on the FRDM-K22F and then it acts like a Segger J-Link (see as well &lt;A href="https://mcuoneclipse.com/2014/04/27/segger-j-link-firmware-for-opensdav2/" title="https://mcuoneclipse.com/2014/04/27/segger-j-link-firmware-for-opensdav2/"&gt;https://mcuoneclipse.com/2014/04/27/segger-j-link-firmware-for-opensdav2/&lt;/A&gt; , but it is for K64F, the same applies pretty much to the K22F).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a look at &lt;A href="http://nxp.com/opensda" title="http://nxp.com/opensda"&gt;OpenSDA Serial and Debug Adapter|NXP&lt;/A&gt;&amp;nbsp; about all the OpenSDA information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 May 2016 20:05:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-OpenOCD-supported-now-for-the-MacOSX/m-p/478697#M5379</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-05-17T20:05:55Z</dc:date>
    </item>
    <item>
      <title>Re: Is OpenOCD supported now for the MacOSX</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-OpenOCD-supported-now-for-the-MacOSX/m-p/478698#M5380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks... after a few fits and starts I finally decided to uninstall KDS and ensure that the Segger OpenSDA was installed properly by dragging the bin (JLink_OpenSDA_V2_1_2015-10-13.bin) to the bootloader folder on the Mac file system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I reinstalled KDS and tried a few example projects all is well!&amp;nbsp; I have to say it is fantastic to be able to develop on the Mac after all these years.&amp;nbsp; The FRDM-K22F and being able to just debug with a USB cable is wonderful!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 May 2016 23:16:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-OpenOCD-supported-now-for-the-MacOSX/m-p/478698#M5380</guid>
      <dc:creator>aerodame</dc:creator>
      <dc:date>2016-05-17T23:16:56Z</dc:date>
    </item>
  </channel>
</rss>