<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: MQX Kernel Data Windows Shows Floating Point IO as No</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/MQX-Kernel-Data-Windows-Shows-Floating-Point-IO-as-No/m-p/478400#M5354</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sol,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is KSDK 1.2 (so the MQX that comes with it).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My floating point printing works fine - shows up in console - so those links aren't what I was looking for.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MQX Kernel Data tab (you can access it via KDS in the Menu MQX...Kernel Data)&amp;nbsp; shows that Floating Point IO is 'No'.&lt;/P&gt;&lt;P&gt;Wondering if it's a bug in the tab or if I didn't do something right.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Raj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jan 2016 01:40:16 GMT</pubDate>
    <dc:creator>rajbatra</dc:creator>
    <dc:date>2016-01-13T01:40:16Z</dc:date>
    <item>
      <title>MQX Kernel Data Windows Shows Floating Point IO as No</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/MQX-Kernel-Data-Windows-Shows-Floating-Point-IO-as-No/m-p/478398#M5352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've compiled MQX with floating point support (here's my userconfig.h):&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#ifndef __user_config_h__&lt;/P&gt;&lt;P&gt;#define __user_config_h__&lt;/P&gt;&lt;P&gt;/* Define user specific modifications of default configuration*/&lt;/P&gt;&lt;P&gt;#define BSPCFG_HAS_SRAM_POOL&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #7ed529;"&gt;#define MQXCFG_ENABLE_FP&amp;nbsp; 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #7ed529;"&gt;#define MQX_INCLUDE_FLOATING_POINT_IO 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;/* include platform-specific configuration */&lt;/P&gt;&lt;P&gt;#include "mqx_cnfg.h"&lt;/P&gt;&lt;P&gt;#endif /* __user_config_h__ */&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, when I view the MQX Kernel Data screen, it states Floating Point IO as No.&lt;/P&gt;&lt;P&gt;I'm using KDS 3.0.x (haven't upgraded to 3.1 yet).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Question: Is the Kernel Data screen wrong, or did I compile it incorrectly?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, my CPU Type shows as Unknown (0x0000) - I'm on a K64.&lt;/P&gt;&lt;P&gt;Attached is a screen shot. Would be curious what others are seeing here when they've enabled floating point IO.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jan 2016 00:00:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/MQX-Kernel-Data-Windows-Shows-Floating-Point-IO-as-No/m-p/478398#M5352</guid>
      <dc:creator>rajbatra</dc:creator>
      <dc:date>2016-01-09T00:00:50Z</dc:date>
    </item>
    <item>
      <title>Re: MQX Kernel Data Windows Shows Floating Point IO as No</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/MQX-Kernel-Data-Windows-Shows-Floating-Point-IO-as-No/m-p/478399#M5353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Raj,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which MQX version are you using??&lt;/P&gt;&lt;P&gt;Please check the below threads and let me know if this helps&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/342693"&gt;printf() with float values&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/355006"&gt;KDS v3.0.0: Floatting point library&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/346841"&gt;Printing Floating point values to fsl_debug_console FRDM-K64F&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 22:14:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/MQX-Kernel-Data-Windows-Shows-Floating-Point-IO-as-No/m-p/478399#M5353</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-01-12T22:14:18Z</dc:date>
    </item>
    <item>
      <title>Re: MQX Kernel Data Windows Shows Floating Point IO as No</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/MQX-Kernel-Data-Windows-Shows-Floating-Point-IO-as-No/m-p/478400#M5354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sol,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is KSDK 1.2 (so the MQX that comes with it).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My floating point printing works fine - shows up in console - so those links aren't what I was looking for.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MQX Kernel Data tab (you can access it via KDS in the Menu MQX...Kernel Data)&amp;nbsp; shows that Floating Point IO is 'No'.&lt;/P&gt;&lt;P&gt;Wondering if it's a bug in the tab or if I didn't do something right.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Raj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2016 01:40:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/MQX-Kernel-Data-Windows-Shows-Floating-Point-IO-as-No/m-p/478400#M5354</guid>
      <dc:creator>rajbatra</dc:creator>
      <dc:date>2016-01-13T01:40:16Z</dc:date>
    </item>
  </channel>
</rss>