<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TWR_K64F120/KDS in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K64F120-KDS/m-p/474218#M5246</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was able to successfully built and run/debug the hello_world_twrk64f120m example project from SDK&amp;nbsp; for the KDS.&lt;/P&gt;&lt;P&gt;I 'm able to debug and flash LEDs however I am not sure how to display the string "hello_world" . I see in the code that UART1 is configured at 115200 bps and is used as debug port .&lt;/P&gt;&lt;P&gt;There is a virtual com port which on my PC is com4 and there is jumpers on TWR_k64f120m that connects the UART1's TX/RX to this virtual port.&lt;/P&gt;&lt;P&gt;So I set the jumpers on the board and open a terminal and nothing is displayed .&lt;/P&gt;&lt;P&gt;Do I need to connect to the actual TX/RX pins of the UART1 on TWR_64K120 board and then connect to the com port on my PC using a USB/RS232 jack?&lt;/P&gt;&lt;P&gt;This virtual com port is a bit confusing for me.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your guidance.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Jan 2016 19:57:58 GMT</pubDate>
    <dc:creator>kooroshhajiani</dc:creator>
    <dc:date>2016-01-29T19:57:58Z</dc:date>
    <item>
      <title>TWR_K64F120/KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K64F120-KDS/m-p/474218#M5246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was able to successfully built and run/debug the hello_world_twrk64f120m example project from SDK&amp;nbsp; for the KDS.&lt;/P&gt;&lt;P&gt;I 'm able to debug and flash LEDs however I am not sure how to display the string "hello_world" . I see in the code that UART1 is configured at 115200 bps and is used as debug port .&lt;/P&gt;&lt;P&gt;There is a virtual com port which on my PC is com4 and there is jumpers on TWR_k64f120m that connects the UART1's TX/RX to this virtual port.&lt;/P&gt;&lt;P&gt;So I set the jumpers on the board and open a terminal and nothing is displayed .&lt;/P&gt;&lt;P&gt;Do I need to connect to the actual TX/RX pins of the UART1 on TWR_64K120 board and then connect to the com port on my PC using a USB/RS232 jack?&lt;/P&gt;&lt;P&gt;This virtual com port is a bit confusing for me.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your guidance.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jan 2016 19:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K64F120-KDS/m-p/474218#M5246</guid>
      <dc:creator>kooroshhajiani</dc:creator>
      <dc:date>2016-01-29T19:57:58Z</dc:date>
    </item>
    <item>
      <title>Re: TWR_K64F120/KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K64F120-KDS/m-p/474219#M5247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Koorosh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Please be sure the virtual com port and the actual UART on your board is which UART, about how&lt;/P&gt;&lt;P&gt;to check which port , you can refer to here &lt;A href="https://community.nxp.com/docs/DOC-329564"&gt;How to use printf() to print string to UART in KDS3.0 + KSDK1.3&lt;/A&gt;&amp;nbsp; about the chapter 2-&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt; Chapter 2 introduces how to check which UART port is used when use printf() to print string on the FRDM board and TOWER board . &lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;- About this TWR-K64F120 board , if you want use the virtual com to print , please connect the 2-3 of J10 and also connect 2-3 of j15 .&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/35932i24B52844F85437D9/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Feb 2016 02:32:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K64F120-KDS/m-p/474219#M5247</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-02-01T02:32:14Z</dc:date>
    </item>
    <item>
      <title>Re: TWR_K64F120/KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K64F120-KDS/m-p/474220#M5248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Alice,&lt;/P&gt;&lt;P&gt;I have the hello world demo working on&amp;nbsp; TWR_K64f120 board.I can communicate over UART1&amp;nbsp; to the PC virtual com port using open SDA USB&lt;/P&gt;&lt;P&gt;For the next step I connected this board to TWR-SER2 board using primary/secondary TWR board.&lt;/P&gt;&lt;P&gt;My intension is to use the DB9 connector on SER2 board via&amp;nbsp; USB-COM jack to communicate to the PC over the serial port.&lt;/P&gt;&lt;P&gt;Now the Demo "Hello World" uses UART1 on the TWR_K64f120 board&amp;nbsp; however the connection between K64f120 and SER2 board via the TWR is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt; font-family: ArialMT;"&gt;Connect MCU’s UART1_RX to primary Elevator (A41)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt; font-family: ArialMT;"&gt;Connect MCU’s UART1_RX to primary Elevator (A42)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt; font-family: ArialMT;"&gt;Which are UART0 RX/TX pins.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Is it possible to connect UART1 pins of the TWR_K64F10 to the UART1 pins of the SER2&amp;nbsp; board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My understanding is that the SER2 DB9 connector is wired to UART1 and&amp;nbsp; K64F120 UART1 goes either to open SDA virtual com port or the UART0 of the primary TWR.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;Do I NEED TO WRITE CODE FOR THE SER2 TO MIRROR UART0 TO UART1?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt; font-family: ArialMT;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Feb 2016 16:31:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K64F120-KDS/m-p/474220#M5248</guid>
      <dc:creator>kooroshhajiani</dc:creator>
      <dc:date>2016-02-03T16:31:18Z</dc:date>
    </item>
  </channel>
</rss>