<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Periodic Interrupt Source - which timer is best? in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Periodic-Interrupt-Source-which-timer-is-best/m-p/473542#M5237</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello STEVE,&lt;/P&gt;&lt;P&gt;If you only use the timer interrupt function , the three module all can&amp;nbsp; generates an interrupt every millisecond.&lt;/P&gt;&lt;P&gt;While the TPM mode can generate PWM signal ,Input capture mode and output compare ;&lt;/P&gt;&lt;P&gt;The PIT mode can generate DMA trigger pulses, only can be sued&amp;nbsp; to the&amp;nbsp; time cunt ;&lt;/P&gt;&lt;P&gt;The LPTMR can run at the five mode : Run, Wait , Stop, Low-Leakage, Debug .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So i think , if you only want generates an interrupt every millisecond , the PIT is enough, for&lt;/P&gt;&lt;P&gt;it can configuration&amp;nbsp; easily .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Mar 2016 04:08:34 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2016-03-14T04:08:34Z</dc:date>
    <item>
      <title>Periodic Interrupt Source - which timer is best?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Periodic-Interrupt-Source-which-timer-is-best/m-p/473541#M5236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am asking this out of general interest:&lt;/P&gt;&lt;P&gt;My application includes a 1 millisecond timer, which obviously generates an interrupt every millisecond.&lt;/P&gt;&lt;P&gt;When I create a Periodic Timer with Processor Expert, I am presented with a number of options for the Periodic Interrupt Source.:&lt;/P&gt;&lt;P&gt;1. One of the Timer/PWM Channels&lt;/P&gt;&lt;P&gt;2. One of the Periodic Interrupt Timers&lt;/P&gt;&lt;P&gt;3. Low Power Timer&lt;/P&gt;&lt;P&gt;But does anyone have some guidance on what is the "preferred" interrupt source?&lt;/P&gt;&lt;P&gt;What advantages does any option have over another?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(PS: for the record, I am working on KL26 and KL03 processors)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Mar 2016 02:03:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Periodic-Interrupt-Source-which-timer-is-best/m-p/473541#M5236</guid>
      <dc:creator>Jiun_Yong</dc:creator>
      <dc:date>2016-03-14T02:03:53Z</dc:date>
    </item>
    <item>
      <title>Re: Periodic Interrupt Source - which timer is best?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Periodic-Interrupt-Source-which-timer-is-best/m-p/473542#M5237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello STEVE,&lt;/P&gt;&lt;P&gt;If you only use the timer interrupt function , the three module all can&amp;nbsp; generates an interrupt every millisecond.&lt;/P&gt;&lt;P&gt;While the TPM mode can generate PWM signal ,Input capture mode and output compare ;&lt;/P&gt;&lt;P&gt;The PIT mode can generate DMA trigger pulses, only can be sued&amp;nbsp; to the&amp;nbsp; time cunt ;&lt;/P&gt;&lt;P&gt;The LPTMR can run at the five mode : Run, Wait , Stop, Low-Leakage, Debug .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So i think , if you only want generates an interrupt every millisecond , the PIT is enough, for&lt;/P&gt;&lt;P&gt;it can configuration&amp;nbsp; easily .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Mar 2016 04:08:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Periodic-Interrupt-Source-which-timer-is-best/m-p/473542#M5237</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-03-14T04:08:34Z</dc:date>
    </item>
  </channel>
</rss>