<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: Debug views in KDS 3.0.0</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Debug-views-in-KDS-3-0-0/m-p/472735#M5223</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Frank,&lt;/P&gt;&lt;P&gt;Yes by default MQX is using lightweight memory pool.&amp;nbsp; This pool is the dynamic memory available to the RTOS and Application and is the heap.&amp;nbsp; By design once the RTOS has instantiated itself and global variables (and other static variables) have been defined SRAM location, the rest of memory gets allocated for heap.&amp;nbsp; Again by default.&amp;nbsp; If your application doesn't need all that space you can make the heap smaller in the linker file (going by memory).&lt;/P&gt;&lt;P&gt;The TAD (Task Aware Debugging) will display stuff for RTOS features that are enabled and not for features that are disabled.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Feb 2016 17:26:55 GMT</pubDate>
    <dc:creator>DavidS</dc:creator>
    <dc:date>2016-02-19T17:26:55Z</dc:date>
    <item>
      <title>Debug views in KDS 3.0.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Debug-views-in-KDS-3-0-0/m-p/472734#M5222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I use KDS 3.0.0 with TWR-K65F180M and KSDK 1.3.0. On debugging there are several&amp;nbsp; views to monitor internal of MQX.&lt;/P&gt;&lt;P&gt;My question is, some views show no information and less show a message like "MessagePool is not installed"(see screen attached). What is to do that I get these information. Is something to install on KDS or on software side on K65?&lt;/P&gt;&lt;P&gt;I have seen that the view for "MQX LightWheight Memory Pools" are available (see screen attached) but I use the MQX as in your example projects and I thinks (I'm sure) it is configured as MQX light weight. It is correct so as it is?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another question is, I have seen that the "MQX LightWheight Memory Pools" show a size of 127,3KB. We use the internal RAM (256KB) only (no external RAM). I think that is a lot! I this the size what the MQX heap is used? When I use MQX-LightWheigt is it more less? How much do you think? Actually we have problems with the less memory heap with our application and want to save heap. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 09:06:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Debug-views-in-KDS-3-0-0/m-p/472734#M5222</guid>
      <dc:creator>frankschuetz</dc:creator>
      <dc:date>2016-02-19T09:06:59Z</dc:date>
    </item>
    <item>
      <title>Re: Debug views in KDS 3.0.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Debug-views-in-KDS-3-0-0/m-p/472735#M5223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Frank,&lt;/P&gt;&lt;P&gt;Yes by default MQX is using lightweight memory pool.&amp;nbsp; This pool is the dynamic memory available to the RTOS and Application and is the heap.&amp;nbsp; By design once the RTOS has instantiated itself and global variables (and other static variables) have been defined SRAM location, the rest of memory gets allocated for heap.&amp;nbsp; Again by default.&amp;nbsp; If your application doesn't need all that space you can make the heap smaller in the linker file (going by memory).&lt;/P&gt;&lt;P&gt;The TAD (Task Aware Debugging) will display stuff for RTOS features that are enabled and not for features that are disabled.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 17:26:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Debug-views-in-KDS-3-0-0/m-p/472735#M5223</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2016-02-19T17:26:55Z</dc:date>
    </item>
  </channel>
</rss>