<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: Error debugging KE04Z in KDS 3.2.0</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Error-debugging-KE04Z-in-KDS-3-2-0/m-p/472395#M5216</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;okay, I think I have this solved so I will post here the answer in case it helps anyone else...&lt;/P&gt;&lt;P&gt;When I had set up my Processor Expert Project, I had selected the KE04Z128M target MCU as that was what I thought I was going to use originally. When I switched over to the FRDM-KE04Z, I neglected to change my target device to the KE04Z8M4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once I made sure that the Target Device (inside of Debug Configurations, Debugger Tab, Select Device) matched my development board, I was able to successfully download my image and debug.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 14 May 2016 15:45:18 GMT</pubDate>
    <dc:creator>jessaskey</dc:creator>
    <dc:date>2016-05-14T15:45:18Z</dc:date>
    <item>
      <title>Error debugging KE04Z in KDS 3.2.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Error-debugging-KE04Z-in-KDS-3-2-0/m-p/472394#M5215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there...&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Im running KDS 3.2.0 under Windows 10 along with a KE04Z. My first program is to flash the Blue LED every 1 second. I have a Processor Expert project set up, debugging configured with my Device showing on USB in the Debugging config ( USB1 - OpenSDA), the FRDM is running the debug app (DEBUG-APP_Pemicro_v107.SDA - Solid Green LED ). When I Run my Debug Configuration.. I get this output...&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Initializing.&lt;/P&gt;&lt;P&gt;Target has been RESET and is active.&lt;/P&gt;&lt;P&gt;CMD&amp;gt;CM D:\Freescale\KDS_v3\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.3.6.201602211227\win32\gdi\P&amp;amp;E\supportFiles_ARM\NXP\KEx\freescale_ke04z128m4_pflash.arp&lt;/P&gt;&lt;P&gt;Initializing.&lt;/P&gt;&lt;P&gt;Initialized.&lt;/P&gt;&lt;P&gt;;version 1.03, 06/02/2014, Copyright 2014 P&amp;amp;E Microcomputer Systems, Inc. All rights reserved. &lt;A href="https://community.nxp.com/www.pemicro.com" target="test_blank"&gt;www.pemicro.com&lt;/A&gt; [ke_128k_pflash_ftmre_m0]&lt;/P&gt;&lt;P&gt;;device freescale, ke04z128m4, pflash&lt;/P&gt;&lt;P&gt;;begin_cs device=$00000000, length=$00020000, ram=$20000000&lt;/P&gt;&lt;P&gt;Loading programming algorithm ... &lt;/P&gt;&lt;P&gt;Error loading .ARP file : D:\Freescale\KDS_v3\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.3.6.201602211227\win32\gdi\P&amp;amp;E\supportFiles_ARM\NXP\KEx\freescale_ke04z128m4_pflash.arp at address 1FFFF000&lt;/P&gt;&lt;P&gt;Error loading programming algorithm - load aborted.&lt;/P&gt;&lt;P&gt;Error occured during Flash programming.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, I have verified that the .arp file above exists in the location. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this a permission issue since Im on a different drive? Windows 10 issue? Other issue?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyone have any hints?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you!&lt;/P&gt;&lt;P&gt;Jess&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 May 2016 04:25:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Error-debugging-KE04Z-in-KDS-3-2-0/m-p/472394#M5215</guid>
      <dc:creator>jessaskey</dc:creator>
      <dc:date>2016-05-14T04:25:56Z</dc:date>
    </item>
    <item>
      <title>Re: Error debugging KE04Z in KDS 3.2.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Error-debugging-KE04Z-in-KDS-3-2-0/m-p/472395#M5216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;okay, I think I have this solved so I will post here the answer in case it helps anyone else...&lt;/P&gt;&lt;P&gt;When I had set up my Processor Expert Project, I had selected the KE04Z128M target MCU as that was what I thought I was going to use originally. When I switched over to the FRDM-KE04Z, I neglected to change my target device to the KE04Z8M4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once I made sure that the Target Device (inside of Debug Configurations, Debugger Tab, Select Device) matched my development board, I was able to successfully download my image and debug.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 May 2016 15:45:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Error-debugging-KE04Z-in-KDS-3-2-0/m-p/472395#M5216</guid>
      <dc:creator>jessaskey</dc:creator>
      <dc:date>2016-05-14T15:45:18Z</dc:date>
    </item>
  </channel>
</rss>