<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KDS project build in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-project-build/m-p/468104#M5089</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a KDS project with FreeRtos&amp;nbsp; that is running on a&amp;nbsp; Twr-k64f120 .I&amp;nbsp; needed to implement a CLI or shell&amp;nbsp; for this project. Freertos provides two files for this purpose FreeRtos_CLI.c and FreeRtos_CLI.h that I have added to the subdirectory called FreeRTOS&amp;nbsp; in the project . the path has been added&amp;nbsp; in the includes field of the C/C++ General under Path and Symbols in project properties.&lt;/P&gt;&lt;P&gt;Now I can't build the project without having to clean project first. Seems something wrong with the dependencies.&lt;/P&gt;&lt;P&gt;If I build without clean I get "no rules to make the target for the FreeRtos_CLI.h".&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any Ideas?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Mar 2016 22:33:26 GMT</pubDate>
    <dc:creator>kooroshhajiani</dc:creator>
    <dc:date>2016-03-10T22:33:26Z</dc:date>
    <item>
      <title>KDS project build</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-project-build/m-p/468104#M5089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a KDS project with FreeRtos&amp;nbsp; that is running on a&amp;nbsp; Twr-k64f120 .I&amp;nbsp; needed to implement a CLI or shell&amp;nbsp; for this project. Freertos provides two files for this purpose FreeRtos_CLI.c and FreeRtos_CLI.h that I have added to the subdirectory called FreeRTOS&amp;nbsp; in the project . the path has been added&amp;nbsp; in the includes field of the C/C++ General under Path and Symbols in project properties.&lt;/P&gt;&lt;P&gt;Now I can't build the project without having to clean project first. Seems something wrong with the dependencies.&lt;/P&gt;&lt;P&gt;If I build without clean I get "no rules to make the target for the FreeRtos_CLI.h".&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any Ideas?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Mar 2016 22:33:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-project-build/m-p/468104#M5089</guid>
      <dc:creator>kooroshhajiani</dc:creator>
      <dc:date>2016-03-10T22:33:26Z</dc:date>
    </item>
    <item>
      <title>Re: KDS project build</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-project-build/m-p/468105#M5090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Koorosh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is hard to recognize root cause from general description. Can you share your project?&lt;/P&gt;&lt;P&gt;According to last sentence it can be related in file name case sensitivity.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are reporting&amp;nbsp; "no rules to make the target for the FreeRtos_CLI.h".&lt;/P&gt;&lt;P&gt;But original file is named FreeRTOS_CLI.h (Upper case "TOS").&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Mar 2016 15:31:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-project-build/m-p/468105#M5090</guid>
      <dc:creator>davidjurajda</dc:creator>
      <dc:date>2016-03-11T15:31:44Z</dc:date>
    </item>
  </channel>
</rss>