<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: Migration to SDK2</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Migration-to-SDK2/m-p/468059#M5087</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andrey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the DOC, this words "and then copy in the existing application code into this new project."&lt;/P&gt;&lt;P&gt;meaning only copy the code you write , do not need copy the KSDK drivers.&lt;/P&gt;&lt;P&gt;While i just have a test to migration one&amp;nbsp; KSDK1.3 hello_world demo to KSDK2.0,&lt;/P&gt;&lt;P&gt;it not only simple copy the application code or file to the new project, we need change some place.&lt;/P&gt;&lt;P&gt;For example , some header file name are different,&amp;nbsp; in the KSDK1.3 : "fsl_lptmr_driver.h", in the KSDK2.0 : "fsl_lptmr.h"&lt;/P&gt;&lt;P&gt;Also some macro define also different.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So i recommend you can first create one simple project on ksdk2.0, for one hand , you can refer to your old project&lt;/P&gt;&lt;P&gt;to write your new application. Or you can copy the application code into your new project , then refer the the KSDK1.3 and 2.0 to change the&lt;/P&gt;&lt;P&gt;different names of your code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And another point , there is no PE on KSDK2.0 , the code on KSDK1.3+PE is the same with KSDK1.3 without PE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Feb 2016 11:20:27 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2016-02-18T11:20:27Z</dc:date>
    <item>
      <title>Migration to SDK2</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Migration-to-SDK2/m-p/468058#M5086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Existing project was created with using Processor Expert and&amp;nbsp; SDK 1.3 for IAR.&lt;/P&gt;&lt;P&gt;According to 'Kinetis SDK 2.0 Transition Guide' (3.8 Migrating a KSDK 1.3 project to Kinetis SDK 2.0), after creating of the new SDK2 project it's needed to 'copy the existing &lt;STRONG&gt;application code&lt;/STRONG&gt; into this new project'.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What mins '&lt;STRONG&gt;application code&lt;/STRONG&gt;' particularly? What folders and files and where it's needed to copy? Only 'sourse' folder?&lt;/P&gt;&lt;P&gt;And what of 'Processor Expert' files it's needed to copy?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Andrey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 08:34:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Migration-to-SDK2/m-p/468058#M5086</guid>
      <dc:creator>agor53</dc:creator>
      <dc:date>2016-02-18T08:34:58Z</dc:date>
    </item>
    <item>
      <title>Re: Migration to SDK2</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Migration-to-SDK2/m-p/468059#M5087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andrey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the DOC, this words "and then copy in the existing application code into this new project."&lt;/P&gt;&lt;P&gt;meaning only copy the code you write , do not need copy the KSDK drivers.&lt;/P&gt;&lt;P&gt;While i just have a test to migration one&amp;nbsp; KSDK1.3 hello_world demo to KSDK2.0,&lt;/P&gt;&lt;P&gt;it not only simple copy the application code or file to the new project, we need change some place.&lt;/P&gt;&lt;P&gt;For example , some header file name are different,&amp;nbsp; in the KSDK1.3 : "fsl_lptmr_driver.h", in the KSDK2.0 : "fsl_lptmr.h"&lt;/P&gt;&lt;P&gt;Also some macro define also different.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So i recommend you can first create one simple project on ksdk2.0, for one hand , you can refer to your old project&lt;/P&gt;&lt;P&gt;to write your new application. Or you can copy the application code into your new project , then refer the the KSDK1.3 and 2.0 to change the&lt;/P&gt;&lt;P&gt;different names of your code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And another point , there is no PE on KSDK2.0 , the code on KSDK1.3+PE is the same with KSDK1.3 without PE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 11:20:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Migration-to-SDK2/m-p/468059#M5087</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-02-18T11:20:27Z</dc:date>
    </item>
    <item>
      <title>Re: Migration to SDK2</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Migration-to-SDK2/m-p/468060#M5088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Alice&lt;SPAN class="font-color-meta" style="padding: 0 0 5px; font-size: 1.2em; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #9aa9af; background-color: #e6e6e6;"&gt;&lt;SPAN class="replyToName" style="font-weight: inherit; font-style: inherit; font-size: 16.8px; font-family: inherit;"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks for your detailed answer, I will try, and I hope it will be enouth.&lt;/P&gt;&lt;P&gt;Andrey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 11:38:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Migration-to-SDK2/m-p/468060#M5088</guid>
      <dc:creator>agor53</dc:creator>
      <dc:date>2016-02-18T11:38:22Z</dc:date>
    </item>
  </channel>
</rss>