<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: undefined reference to 'AS1_OnBlockReceived' when Interrupt service/event box is checked in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/undefined-reference-to-AS1-OnBlockReceived-when-Interrupt/m-p/467187#M5029</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please create one new project , then add&amp;nbsp; the UART to configuration .&lt;/P&gt;&lt;P&gt;I test your project on my side , it also have error when build , while i create&lt;/P&gt;&lt;P&gt;a new project , add the Serial_LDD component , enable the interrupt,&amp;nbsp; it have no error when build.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53554iAAEA73504D534281/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I don't whether there is some problem when you create and configure the project.&lt;/P&gt;&lt;P&gt;I attach my project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Feb 2016 02:50:36 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2016-02-18T02:50:36Z</dc:date>
    <item>
      <title>undefined reference to 'AS1_OnBlockReceived' when Interrupt service/event box is checked</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/undefined-reference-to-AS1-OnBlockReceived-when-Interrupt/m-p/467186#M5028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm using a FRDM-K22F board with the FRDM-STBC-AGM01 shield. Using KDS V3.0.0&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using the sensor fusion example project in:&lt;/P&gt;&lt;P&gt;C:\...\FreescaleSensorFusionRevision5\KDS\KDS3 FRDM 6DOF Bare Board eCompass\FRDM_K22F&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The example code works great. I am able to download and program the FRDM-K22F and fire up the Sensor Fusion GUI. Everything works great.&lt;/P&gt;&lt;P&gt;Then I try and add a Serial_LDD component (aka UART) in PE. I select UART0 and PTD6 and PTD7 for the pins and a baud rate of 115200. I click the PE "Generate code" button and get no errors. I then do a build and get errors:&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121081i21B8A03775174F32/image-size/large?v=v2&amp;amp;px=999" title="141186_141186.png" alt="141186_141186.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53383i3836D0BA3ED3F17E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If I un-check the "Interrupt service/event" box in the component inspector the errors go away but I would like to use the interrupts when a block is sent or received.&lt;/P&gt;&lt;P&gt;How to I get around this error? Project attached.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338764"&gt;FRDM_K22F_With_FRDM-STBC-AGM01.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Feb 2016 16:30:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/undefined-reference-to-AS1-OnBlockReceived-when-Interrupt/m-p/467186#M5028</guid>
      <dc:creator>marks</dc:creator>
      <dc:date>2016-02-17T16:30:55Z</dc:date>
    </item>
    <item>
      <title>Re: undefined reference to 'AS1_OnBlockReceived' when Interrupt service/event box is checked</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/undefined-reference-to-AS1-OnBlockReceived-when-Interrupt/m-p/467187#M5029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please create one new project , then add&amp;nbsp; the UART to configuration .&lt;/P&gt;&lt;P&gt;I test your project on my side , it also have error when build , while i create&lt;/P&gt;&lt;P&gt;a new project , add the Serial_LDD component , enable the interrupt,&amp;nbsp; it have no error when build.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53554iAAEA73504D534281/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I don't whether there is some problem when you create and configure the project.&lt;/P&gt;&lt;P&gt;I attach my project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 02:50:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/undefined-reference-to-AS1-OnBlockReceived-when-Interrupt/m-p/467187#M5029</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-02-18T02:50:36Z</dc:date>
    </item>
    <item>
      <title>Re: undefined reference to 'AS1_OnBlockReceived' when Interrupt service/event box is checked</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/undefined-reference-to-AS1-OnBlockReceived-when-Interrupt/m-p/467188#M5030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice, Thank you for the fast response! I have the same results as you. I created a new project and added two UARTs and enable interrupts. The build went fine with no errors. I also did a build on your project with no errors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did update to KDS 3.1 from 3.0. thinking that might be the problem. Because when i did a&amp;nbsp; help&amp;gt;check for updates in 3.0 and the link was broken for updates, so I uninstalled KDS and re-installed. I tried it again on the Sensor Fusion example code but no change. Even with the newly installed KDS 3.1 I still can not add a UART to the example code. Surly I am not the only one that will run into this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any other thoughts? Can you tell why my project has an error?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help!&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 03:29:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/undefined-reference-to-AS1-OnBlockReceived-when-Interrupt/m-p/467188#M5030</guid>
      <dc:creator>marks</dc:creator>
      <dc:date>2016-02-18T03:29:35Z</dc:date>
    </item>
    <item>
      <title>Re: undefined reference to 'AS1_OnBlockReceived' when Interrupt service/event box is checked</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/undefined-reference-to-AS1-OnBlockReceived-when-Interrupt/m-p/467189#M5031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mark,&lt;/P&gt;&lt;P&gt;Since there is no error in you new project , why do you use the new one ,&lt;/P&gt;&lt;P&gt;then add the other PE component and code into your new project, you can add one then build&lt;/P&gt;&lt;P&gt;once to check whether there have error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 08:15:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/undefined-reference-to-AS1-OnBlockReceived-when-Interrupt/m-p/467189#M5031</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-02-18T08:15:18Z</dc:date>
    </item>
  </channel>
</rss>