<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: FRDM K65 Board feasibility</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/FRDM-K65-Board-feasibility/m-p/466575#M5004</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is feasible really! Even the K65 does not support BLE itself, but you can use the SPI to interface an external bluetooth chip. For Wifi connection, the K65 SDHC really compliance with the SDIO and can been used as WIFI communication. Also, we had the MQX RTCS really supporting thee DHCP and IPV6. Attached picture is a description for the hardware interface.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Feb 2016 07:49:50 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2016-02-25T07:49:50Z</dc:date>
    <item>
      <title>FRDM K65 Board feasibility</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/FRDM-K65-Board-feasibility/m-p/466574#M5003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are planning to select Kinetis K65F board for our project development.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We need to implement all the below features on it.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp; ---&amp;nbsp; Blue tooth and WIFI interfacing&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp; ---&amp;nbsp; Adding external&amp;nbsp; RAM memory to avoid memory concerns.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp; ---&amp;nbsp; DHCP and IPV6 Implementation&lt;/EM&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt; Can anyone tell the feasibility of this board selection.&lt;/STRONG&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Which will be better module option for&lt;STRONG&gt; bluetooth, Wifi and external RAM&lt;/STRONG&gt; interfacing in K65 family&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Feb 2016 10:51:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/FRDM-K65-Board-feasibility/m-p/466574#M5003</guid>
      <dc:creator>rahul_eris</dc:creator>
      <dc:date>2016-02-17T10:51:29Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM K65 Board feasibility</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/FRDM-K65-Board-feasibility/m-p/466575#M5004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is feasible really! Even the K65 does not support BLE itself, but you can use the SPI to interface an external bluetooth chip. For Wifi connection, the K65 SDHC really compliance with the SDIO and can been used as WIFI communication. Also, we had the MQX RTCS really supporting thee DHCP and IPV6. Attached picture is a description for the hardware interface.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Feb 2016 07:49:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/FRDM-K65-Board-feasibility/m-p/466575#M5004</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-02-25T07:49:50Z</dc:date>
    </item>
  </channel>
</rss>