<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックProject-file subdir.mk not up to date!</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Project-file-subdir-mk-not-up-to-date/m-p/462701#M4866</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using KDS to create libraries which we use on both M4 and M0+, and they all exist in Debug and Release versions.&lt;/P&gt;&lt;P&gt;Today I found that my M4-Debug version (M4-Debug\mmSrc\MMComm\subdir.mk) has more files than the M0-version!!!&lt;/P&gt;&lt;P&gt;It seems that the subdir.mk is only updated on the actual build target?&lt;/P&gt;&lt;P&gt;Is this right or am I missing something?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Dec 2015 07:35:48 GMT</pubDate>
    <dc:creator>oaf</dc:creator>
    <dc:date>2015-12-04T07:35:48Z</dc:date>
    <item>
      <title>Project-file subdir.mk not up to date!</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Project-file-subdir-mk-not-up-to-date/m-p/462701#M4866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using KDS to create libraries which we use on both M4 and M0+, and they all exist in Debug and Release versions.&lt;/P&gt;&lt;P&gt;Today I found that my M4-Debug version (M4-Debug\mmSrc\MMComm\subdir.mk) has more files than the M0-version!!!&lt;/P&gt;&lt;P&gt;It seems that the subdir.mk is only updated on the actual build target?&lt;/P&gt;&lt;P&gt;Is this right or am I missing something?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Dec 2015 07:35:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Project-file-subdir-mk-not-up-to-date/m-p/462701#M4866</guid>
      <dc:creator>oaf</dc:creator>
      <dc:date>2015-12-04T07:35:48Z</dc:date>
    </item>
    <item>
      <title>Re: Project-file subdir.mk not up to date!</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Project-file-subdir-mk-not-up-to-date/m-p/462702#M4867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;subdir.mk is Automatically-generated file after build.&lt;/P&gt;&lt;P&gt;can you please:&lt;/P&gt;&lt;P&gt;1. manually remove it from your project folder.&lt;/P&gt;&lt;P&gt;2, do "project", "clean..." then rebuild your project. this can generate a new subdir.mk file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can it work for you?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Dec 2015 03:25:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Project-file-subdir-mk-not-up-to-date/m-p/462702#M4867</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-12-18T03:25:30Z</dc:date>
    </item>
  </channel>
</rss>