<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: Does Kinetis has a simulator?</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461779#M4826</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Is&amp;nbsp; the uTasker also a simulator that I can use?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 03 Jan 2016 16:10:34 GMT</pubDate>
    <dc:creator>BlueTower</dc:creator>
    <dc:date>2016-01-03T16:10:34Z</dc:date>
    <item>
      <title>Does Kinetis has a simulator?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461777#M4824</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;New to kinetis. Does kinetis Design Studio has a simulator like stepping through the code etc. ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Jan 2016 11:56:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461777#M4824</guid>
      <dc:creator>BlueTower</dc:creator>
      <dc:date>2016-01-03T11:56:46Z</dc:date>
    </item>
    <item>
      <title>Re: Does Kinetis has a simulator?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461778#M4825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexandros,&lt;/P&gt;&lt;P&gt;a simulator is not included in KDS. But there is QEMU which you could use, see &lt;A href="http://gnuarmeclipse.github.io/qemu/" title="http://gnuarmeclipse.github.io/qemu/"&gt;The GNU ARM Eclipse QEMU&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Jan 2016 12:26:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461778#M4825</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-01-03T12:26:05Z</dc:date>
    </item>
    <item>
      <title>Re: Does Kinetis has a simulator?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461779#M4826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Is&amp;nbsp; the uTasker also a simulator that I can use?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Jan 2016 16:10:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461779#M4826</guid>
      <dc:creator>BlueTower</dc:creator>
      <dc:date>2016-01-03T16:10:34Z</dc:date>
    </item>
    <item>
      <title>Re: Does Kinetis has a simulator?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461780#M4827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexandros,&lt;/P&gt;&lt;P&gt;yes, that's another simulator you can use.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Jan 2016 17:10:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461780#M4827</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-01-03T17:10:33Z</dc:date>
    </item>
    <item>
      <title>Re: Does Kinetis has a simulator?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461781#M4828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/322132"&gt;New Freedom FRDM-K64F board&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is pre-built simulator at that link which can be tried [it takes about 30..40s from clicking the download link to running a virtual FRDM-K64F with Ethernet, Web server, Telenet, SD card and USB (although Winpcap should be installed on the PC due to its DLL being needed - it is already there if Wireshark has been installed].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Jan 2016 23:23:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461781#M4828</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-01-03T23:23:41Z</dc:date>
    </item>
    <item>
      <title>Re: Does Kinetis has a simulator?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461782#M4829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does Codewarrior for K series mcu's provides simulation for the K64P144M120SF5RM which is a FRDM-K64F device?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jan 2016 21:16:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461782#M4829</guid>
      <dc:creator>BlueTower</dc:creator>
      <dc:date>2016-01-05T21:16:17Z</dc:date>
    </item>
    <item>
      <title>Re: Does Kinetis has a simulator?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461783#M4830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexandros,&lt;/P&gt;&lt;P&gt;CodeWarrior for MCU does not include a simulator for ARM. Options are the ones outlined in this thread. Keep in mind that even these similator are mostly core simulator and do not simulate the full device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jan 2016 05:50:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461783#M4830</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-01-06T05:50:08Z</dc:date>
    </item>
    <item>
      <title>Re: Does Kinetis has a simulator?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461784#M4831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Is there any simulator for kinetis, which can simulate the full device?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Mar 2017 06:09:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461784#M4831</guid>
      <dc:creator>vignesh_vb_7</dc:creator>
      <dc:date>2017-03-20T06:09:18Z</dc:date>
    </item>
    <item>
      <title>Re: Does Kinetis has a simulator?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461785#M4832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vignesh,&lt;/P&gt;&lt;P&gt;I'm aware of the following two:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://gnuarmeclipse.github.io/qemu/" title="http://gnuarmeclipse.github.io/qemu/"&gt;The GNU ARM Eclipse QEMU&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.utasker.com/Demos/Simulations.html" title="http://www.utasker.com/Demos/Simulations.html"&gt;µTasker - Simulation examples&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Mar 2017 07:00:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Does-Kinetis-has-a-simulator/m-p/461785#M4832</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-03-20T07:00:32Z</dc:date>
    </item>
  </channel>
</rss>