<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックInterrupt in kl46Z</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Interrupt-in-kl46Z/m-p/457768#M4729</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on freedom KL46Z board using interrupt on KDS3.0 with KSDK1.2.0&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;switch SW1 on freedom board is connected to PTC-3 and SW2 is conected to PTC-12 port pin&lt;/P&gt;&lt;P&gt;i have enable interrupts for the SW1 and SW2 on processor expert&lt;/P&gt;&lt;P&gt;when i generate a code i can see Events.c as below&lt;/P&gt;&lt;P&gt;void PORTC_PORTD_IRQHandler(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; PORT_HAL_ClearPortIntFlag(PORTC_BASE_PTR);&lt;/P&gt;&lt;P&gt; /* Write your code here ... */&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;how can i access individual interrupt from SW1 or SW2&lt;/P&gt;&lt;P&gt;i tried to identify interrupt from SW1 from function: GPIO_DRV_ReadPinInput(BUTTON_SW1)&lt;/P&gt;&lt;P&gt;but not able to identify the interrupt is from the source SW1 or SW2 ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;can any one has come across this scenario?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Aug 2015 13:48:03 GMT</pubDate>
    <dc:creator>bheemarao</dc:creator>
    <dc:date>2015-08-21T13:48:03Z</dc:date>
    <item>
      <title>Interrupt in kl46Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Interrupt-in-kl46Z/m-p/457768#M4729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on freedom KL46Z board using interrupt on KDS3.0 with KSDK1.2.0&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;switch SW1 on freedom board is connected to PTC-3 and SW2 is conected to PTC-12 port pin&lt;/P&gt;&lt;P&gt;i have enable interrupts for the SW1 and SW2 on processor expert&lt;/P&gt;&lt;P&gt;when i generate a code i can see Events.c as below&lt;/P&gt;&lt;P&gt;void PORTC_PORTD_IRQHandler(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; PORT_HAL_ClearPortIntFlag(PORTC_BASE_PTR);&lt;/P&gt;&lt;P&gt; /* Write your code here ... */&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;how can i access individual interrupt from SW1 or SW2&lt;/P&gt;&lt;P&gt;i tried to identify interrupt from SW1 from function: GPIO_DRV_ReadPinInput(BUTTON_SW1)&lt;/P&gt;&lt;P&gt;but not able to identify the interrupt is from the source SW1 or SW2 ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;can any one has come across this scenario?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 13:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Interrupt-in-kl46Z/m-p/457768#M4729</guid>
      <dc:creator>bheemarao</dc:creator>
      <dc:date>2015-08-21T13:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt in kl46Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Interrupt-in-kl46Z/m-p/457769#M4730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bheema,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to call the function PORT_HAL_IsPinIntPending (the second parameter is the pin) before to clear the flag.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code _jivemacro_uid_14401872974191602 jive_text_macro" data-renderedposition="134_8_1231_128" jivemacro_uid="_14401872974191602" modifiedtitle="true"&gt;&lt;P&gt;void PORTC_PORTD_IRQHandler(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; if(PORT_HAL_IsPinIntPending(PORTC_BASE_PTR, 3))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_ClearPinIntFlag(PORTC_BASE_PTR, 3);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Write your code here ... */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #eb7a3d;"&gt;&lt;STRONG&gt;/* If this post answers your question please click the Correct Answer button. */&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 20:04:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Interrupt-in-kl46Z/m-p/457769#M4730</guid>
      <dc:creator>EarlOrlando</dc:creator>
      <dc:date>2015-08-21T20:04:42Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt in kl46Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Interrupt-in-kl46Z/m-p/457770#M4731</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes it worked fine for me.&lt;/P&gt;&lt;P&gt;Thanks for sharing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2015 05:38:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Interrupt-in-kl46Z/m-p/457770#M4731</guid>
      <dc:creator>bheemarao</dc:creator>
      <dc:date>2015-08-24T05:38:58Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt in kl46Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Interrupt-in-kl46Z/m-p/457771#M4732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The mistake i was making is: i was clearing the interrupt flag using&amp;nbsp; " GPIO_DRV_ClearPinIntFlag(BUTTON_SW2);" which was not working i believe, we have to clear flag using "PORT_HAL_ClearPortIntFlag(PORTC_BASE_PTR);"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if(GPIO_DRV_IsPinIntPending(BUTTON_SW2)!=1){&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; GPIO_DRV_TogglePinOutput(LED2_RED);&lt;/P&gt;&lt;P&gt;&amp;nbsp; // GPIO_DRV_ClearPinIntFlag(BUTTON_SW2);&amp;nbsp; //wrong way of clearing int flag&lt;/P&gt;&lt;P&gt;PORT_HAL_ClearPortIntFlag(PORTC_BASE_PTR);&amp;nbsp; // correct way which is working fine&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and instead of using the HAL " &lt;SPAN style="font-size: 12px; font-family: Consolas, 'Courier New', Courier, mono, serif; color: #000000;"&gt;PORT_HAL_IsPinIntPending(PORTC_BASE_PTR, &lt;/SPAN&gt;&lt;SPAN class="number" style="font-size: 12px; font-family: Consolas, 'Courier New', Courier, mono, serif; color: green;"&gt;3&lt;/SPAN&gt;&lt;SPAN style="font-size: 12px; font-family: Consolas, 'Courier New', Courier, mono, serif; color: #000000;"&gt;)" we can use "GPIO_DRV_IsPinIntPending(BUTTON_SW2)" which is user friendly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2015 06:48:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Interrupt-in-kl46Z/m-p/457771#M4732</guid>
      <dc:creator>bheemarao</dc:creator>
      <dc:date>2015-08-24T06:48:51Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt in kl46Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Interrupt-in-kl46Z/m-p/457772#M4733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also we can control multiple pin interrupt requests for the same port. There is an example code below which written directly to relevant registers for frdm_kl46z.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12px;"&gt;void PORTC_PORTD_IRQHandler(void){&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12px;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;switch((uint32_t)PORTC_ISFR)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // to determine pin number look into PORTC_ISFR register.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;{ &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;case ((uint32_t)1&amp;lt;&amp;lt;SW1) : &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;// if SW1 button pressed&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;PORTC_PCR(SW1) |= PORT_PCR_ISF_MASK; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;// Clear interrupt service flag in port control register otherwise int. remains active &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;GPIOD_PTOR |= GPIO_PTOR_PTTO(GreenLedMask); &amp;nbsp;&amp;nbsp;&amp;nbsp;// toggle Green LED &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;break;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;case ((uint32_t)1&amp;lt;&amp;lt;SW3) : &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;// if SW3 button pressed&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;PORTC_PCR(SW3) |= PORT_PCR_ISF_MASK; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;// Clear interrupt service flag in port control register otherwise int. remains active &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;GPIOD_PTOR |= GPIO_PTOR_PTTO(RedLedMask); &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;// toggle Red LED&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;break;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;default :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;PORTC_ISFR |= (0xFFFFFFFF);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;// clear all flags to prevent being stuck in repetitive interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;SPAN&gt;GPIOD_PTOR |= GPIO_PTOR_PTTO(RedLedMask);&lt;/SPAN&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;// toggle Red LED&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;SPAN&gt;GPIOD_PTOR |= GPIO_PTOR_PTTO(GreenLedMask);&lt;/SPAN&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp;// toggle Green LED&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 12px;"&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;break;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12px;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12px;"&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12px;"&gt;and definitions like this :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12px;"&gt;#define RedLED &amp;nbsp;&amp;nbsp;&amp;nbsp;29&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;// PTE pin 29&lt;BR /&gt;#define GreenLED 5 &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;// PTD pin 5&lt;BR /&gt;#define SW1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 3&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // PTC pin 3&lt;BR /&gt;#define SW3 &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;12 &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;// PTC pin 12&lt;BR /&gt;#define PORTC_D_IRQ_NBR (IRQn_Type)31 // IRQ number&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12px;"&gt;const uint32_t GreenLedMask = (1&amp;lt;&amp;lt;GreenLED);&lt;BR /&gt;const uint32_t RedLedMask &amp;nbsp;&amp;nbsp;&amp;nbsp; = (1&amp;lt;&amp;lt;RedLED);&lt;BR /&gt;const uint32_t SW1Mask &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= (1&amp;lt;&amp;lt;SW1);&lt;BR /&gt;const uint32_t SW3Mask &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= (1&amp;lt;&amp;lt;SW3);&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Dec 2016 12:58:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Interrupt-in-kl46Z/m-p/457772#M4733</guid>
      <dc:creator>yusufyelkovan</dc:creator>
      <dc:date>2016-12-21T12:58:00Z</dc:date>
    </item>
  </channel>
</rss>