<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Port Control Registers not in header file in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Port-Control-Registers-not-in-header-file/m-p/456444#M4681</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Zachary,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes , in the header file of "MK20D7.h", it doesn't directly define the PORTx_PCRn.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1) While we can use the struct of register to show , for example :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTA-&amp;gt;PCR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) If you have CW , we also can refer to the header file of CW, copy the definition of PORTx_PCRn to the header file of KDS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36704iD7EC25ABE5D6058C/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 May 2015 02:24:59 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2015-05-26T02:24:59Z</dc:date>
    <item>
      <title>Port Control Registers not in header file</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Port-Control-Registers-not-in-header-file/m-p/456443#M4680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm a new here, just getting started with the Kinetis Design Studio using a MK20DX256VLH7 controller.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The manual refers to Port Control Registers such as PORTx_PCRn but they do not seem to be available. The IDE automatically included "MK20D7.h"&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a file I am missing? Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2015 10:21:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Port-Control-Registers-not-in-header-file/m-p/456443#M4680</guid>
      <dc:creator>zacharylevenber</dc:creator>
      <dc:date>2015-05-22T10:21:08Z</dc:date>
    </item>
    <item>
      <title>Re: Port Control Registers not in header file</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Port-Control-Registers-not-in-header-file/m-p/456444#M4681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Zachary,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes , in the header file of "MK20D7.h", it doesn't directly define the PORTx_PCRn.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1) While we can use the struct of register to show , for example :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTA-&amp;gt;PCR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) If you have CW , we also can refer to the header file of CW, copy the definition of PORTx_PCRn to the header file of KDS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36704iD7EC25ABE5D6058C/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2015 02:24:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Port-Control-Registers-not-in-header-file/m-p/456444#M4681</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-05-26T02:24:59Z</dc:date>
    </item>
  </channel>
</rss>