<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TSS Settings in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TSS-Settings/m-p/452655#M4579</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I implement a keypad (15 keys) that uses 8 electrodes (3 columns, 5 rows) in KL05 with KDS3.0. Now I have a problem. When I pressed one key, did not release it, then I pressed another key that in the same row or column, that means the two keys shared one electrode, the TSS library can not report the second key. How can I config the PE to implement this feature. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Sep 2015 15:38:03 GMT</pubDate>
    <dc:creator>东升王</dc:creator>
    <dc:date>2015-09-15T15:38:03Z</dc:date>
    <item>
      <title>TSS Settings</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TSS-Settings/m-p/452655#M4579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I implement a keypad (15 keys) that uses 8 electrodes (3 columns, 5 rows) in KL05 with KDS3.0. Now I have a problem. When I pressed one key, did not release it, then I pressed another key that in the same row or column, that means the two keys shared one electrode, the TSS library can not report the second key. How can I config the PE to implement this feature. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Sep 2015 15:38:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/TSS-Settings/m-p/452655#M4579</guid>
      <dc:creator>东升王</dc:creator>
      <dc:date>2015-09-15T15:38:03Z</dc:date>
    </item>
    <item>
      <title>Re: TSS Settings</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TSS-Settings/m-p/452656#M4580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dongsheng&lt;/P&gt;&lt;P&gt;you can check the TSS samples for the TWR board&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_TSS_3_1\examples\TWRKXX_DEMO\build\cw10&lt;/P&gt;&lt;P&gt;please check the section for the keypad2,&lt;/P&gt;&lt;P&gt;I use the k60 and it can detect two number (like 4 and 1) that share one electrode touched at the same time.&lt;/P&gt;&lt;P&gt;Also you can use freemaster to check the delta variation on each electrode, with this variation you can detect the two diferent keys that share the same electrode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Vicente&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2015 18:30:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/TSS-Settings/m-p/452656#M4580</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2015-09-25T18:30:33Z</dc:date>
    </item>
  </channel>
</rss>