<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K10DX128xxx5 nvm eeprom flash in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/K10DX128xxx5-nvm-eeprom-flash/m-p/451252#M4542</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I have tried the checkbox Preserve Partitioning for the device but without any luck? I have tried it in both KDS and codewarrior 10.6.&lt;/P&gt;&lt;P&gt;If I should set any memoryrange for preserving is it correct to set from 0x10000000 to 0x10002000 when I use the MK10DX128 cpu?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have read in another thread that PE micro should make another .arp file for programming the device. I use the latest version from PE Micro version 1.07. Is there any newer version of the file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this is not working is there any other way to debug the chip without erasing the internal EEPROM?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Andreas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 May 2015 06:37:42 GMT</pubDate>
    <dc:creator>andreaswickströ</dc:creator>
    <dc:date>2015-05-21T06:37:42Z</dc:date>
    <item>
      <title>K10DX128xxx5 nvm eeprom flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/K10DX128xxx5-nvm-eeprom-flash/m-p/451250#M4540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Is it posible to download code and debug this cpu without erasing the internal eeprom (nvm memory). I have used a segger and a PE micro debugger without any luck.&lt;/P&gt;&lt;P&gt;I am able to use the memory and it works as long as i dont download new firmware to it.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope someone know how to be able to debug the firmware without erasing the internal eeprom.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Andreas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 17:05:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/K10DX128xxx5-nvm-eeprom-flash/m-p/451250#M4540</guid>
      <dc:creator>andreaswickströ</dc:creator>
      <dc:date>2015-05-20T17:05:02Z</dc:date>
    </item>
    <item>
      <title>Re: K10DX128xxx5 nvm eeprom flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/K10DX128xxx5-nvm-eeprom-flash/m-p/451251#M4541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andreas:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not tried such feature myself, but the latest P&amp;amp;E GDB plugin&amp;nbsp; in KDS v3.0.0 you have the option to preserve memory spaces:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/34319i5AFF4F58EEB5D322/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 May 2015 02:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/K10DX128xxx5-nvm-eeprom-flash/m-p/451251#M4541</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-05-21T02:00:27Z</dc:date>
    </item>
    <item>
      <title>Re: K10DX128xxx5 nvm eeprom flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/K10DX128xxx5-nvm-eeprom-flash/m-p/451252#M4542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I have tried the checkbox Preserve Partitioning for the device but without any luck? I have tried it in both KDS and codewarrior 10.6.&lt;/P&gt;&lt;P&gt;If I should set any memoryrange for preserving is it correct to set from 0x10000000 to 0x10002000 when I use the MK10DX128 cpu?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have read in another thread that PE micro should make another .arp file for programming the device. I use the latest version from PE Micro version 1.07. Is there any newer version of the file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this is not working is there any other way to debug the chip without erasing the internal EEPROM?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Andreas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 May 2015 06:37:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/K10DX128xxx5-nvm-eeprom-flash/m-p/451252#M4542</guid>
      <dc:creator>andreaswickströ</dc:creator>
      <dc:date>2015-05-21T06:37:42Z</dc:date>
    </item>
    <item>
      <title>Re: K10DX128xxx5 nvm eeprom flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/K10DX128xxx5-nvm-eeprom-flash/m-p/451253#M4543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andreas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use the "Targer Tasks" to flash the region you want .&lt;/P&gt;&lt;P&gt;The detail steps please refer to here : &lt;STRONG&gt;&lt;A href="https://community.nxp.com/docs/DOC-102167"&gt;Preserve Memory Ranges In CodeWarrior v10.6&lt;/A&gt; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;And the detail information on CW10.6 you can refer to&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;" ....\CW MCU v10.6\MCU\Help\PDF\CodeWarrior Development Studio Common Features Guide"&lt;/P&gt;&lt;P&gt;-&amp;gt; "3.11 Flash programmer"&amp;nbsp; , especaill the " 3.11.2.3.2 Program/Verify actions "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have test on kinetis k64 chip , if you have any question hen you test this method , please tell me .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2015 02:43:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/K10DX128xxx5-nvm-eeprom-flash/m-p/451253#M4543</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-06-02T02:43:29Z</dc:date>
    </item>
  </channel>
</rss>