<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Memory problems with KDS 3.0 and K64</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Memory-problems-with-KDS-3-0-and-K64/m-p/445971#M4340</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I’m using Kinetis studio 3.0. which I think is wonderful IDE. However I have problem that I hope somebody could help me. In my project I have several arrays and the pretty big, between 1K to 8K of unint8_t and uint16_t. Some of them are local and some are global. Also I have global data for the ISR. I’m developing in a bareboard proyect and I’m using an MK64 with a 1Mb of flash and 256 Kb of RAM. My problem is the next:&lt;/P&gt;&lt;P&gt;I have a global variable called rxUART that contains information for the UART and a FIFO. Also I have an array like this uint16_t pointers [2048]. Everything works ok until I clean the content of pointers, when I do this the values in rxUART goes to zero. It seems like stack stack overflow, however both are global data. The same project works well in code warrior 10.6, so I think I need to configure the memory map for the K64 in the KDS 3.0. Some body can tell how can I do this? I want to use all the memory resource (256K) without heap.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Oct 2015 19:43:58 GMT</pubDate>
    <dc:creator>mikesmith1980</dc:creator>
    <dc:date>2015-10-30T19:43:58Z</dc:date>
    <item>
      <title>Memory problems with KDS 3.0 and K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Memory-problems-with-KDS-3-0-and-K64/m-p/445971#M4340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I’m using Kinetis studio 3.0. which I think is wonderful IDE. However I have problem that I hope somebody could help me. In my project I have several arrays and the pretty big, between 1K to 8K of unint8_t and uint16_t. Some of them are local and some are global. Also I have global data for the ISR. I’m developing in a bareboard proyect and I’m using an MK64 with a 1Mb of flash and 256 Kb of RAM. My problem is the next:&lt;/P&gt;&lt;P&gt;I have a global variable called rxUART that contains information for the UART and a FIFO. Also I have an array like this uint16_t pointers [2048]. Everything works ok until I clean the content of pointers, when I do this the values in rxUART goes to zero. It seems like stack stack overflow, however both are global data. The same project works well in code warrior 10.6, so I think I need to configure the memory map for the K64 in the KDS 3.0. Some body can tell how can I do this? I want to use all the memory resource (256K) without heap.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Oct 2015 19:43:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Memory-problems-with-KDS-3-0-and-K64/m-p/445971#M4340</guid>
      <dc:creator>mikesmith1980</dc:creator>
      <dc:date>2015-10-30T19:43:58Z</dc:date>
    </item>
    <item>
      <title>Re: Memory problems with KDS 3.0 and K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Memory-problems-with-KDS-3-0-and-K64/m-p/445972#M4341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just resolved the problem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 31 Oct 2015 15:11:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Memory-problems-with-KDS-3-0-and-K64/m-p/445972#M4341</guid>
      <dc:creator>mikesmith1980</dc:creator>
      <dc:date>2015-10-31T15:11:06Z</dc:date>
    </item>
    <item>
      <title>Re: Memory problems with KDS 3.0 and K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Memory-problems-with-KDS-3-0-and-K64/m-p/445973#M4342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;Should be nice if you could explain how you fixed the issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jan 2020 18:18:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Memory-problems-with-KDS-3-0-and-K64/m-p/445973#M4342</guid>
      <dc:creator>AlanAssis</dc:creator>
      <dc:date>2020-01-23T18:18:51Z</dc:date>
    </item>
  </channel>
</rss>