<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TWR-K60F120M getting the DAC to work in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K60F120M-getting-the-DAC-to-work/m-p/435800#M3917</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to get the ADC and DAC to run on the TWR-K60F120M. I am using KDS and PE. I added the ADC and it worked like a charm. I can see the zig-zag curve that the wave gen generates when tracing the output variable within FreeMASTER. Now I just looped the output back into the DAC and wanted to see the signal again on the oscilloscope. But the DAC just does not seem to work at all. I used &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fmcuoneclipse.com%2F2013%2F02%2F23%2Fdac-example-with-the-freedom-board%2F" rel="nofollow" target="_blank"&gt;this&lt;/A&gt; example as a starting point.&lt;/P&gt;&lt;P&gt;I tried to use the high level PE component&amp;nbsp; as well as the LDD directly.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did anyone ever try to use the DAC and can possibly help me with any guidance or tips?&lt;/P&gt;&lt;P&gt;Best regards and thanks,&lt;/P&gt;&lt;P&gt;Jan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Sep 2015 09:24:10 GMT</pubDate>
    <dc:creator>jrs1986</dc:creator>
    <dc:date>2015-09-09T09:24:10Z</dc:date>
    <item>
      <title>TWR-K60F120M getting the DAC to work</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K60F120M-getting-the-DAC-to-work/m-p/435800#M3917</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to get the ADC and DAC to run on the TWR-K60F120M. I am using KDS and PE. I added the ADC and it worked like a charm. I can see the zig-zag curve that the wave gen generates when tracing the output variable within FreeMASTER. Now I just looped the output back into the DAC and wanted to see the signal again on the oscilloscope. But the DAC just does not seem to work at all. I used &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fmcuoneclipse.com%2F2013%2F02%2F23%2Fdac-example-with-the-freedom-board%2F" rel="nofollow" target="_blank"&gt;this&lt;/A&gt; example as a starting point.&lt;/P&gt;&lt;P&gt;I tried to use the high level PE component&amp;nbsp; as well as the LDD directly.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did anyone ever try to use the DAC and can possibly help me with any guidance or tips?&lt;/P&gt;&lt;P&gt;Best regards and thanks,&lt;/P&gt;&lt;P&gt;Jan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Sep 2015 09:24:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K60F120M-getting-the-DAC-to-work/m-p/435800#M3917</guid>
      <dc:creator>jrs1986</dc:creator>
      <dc:date>2015-09-09T09:24:10Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60F120M getting the DAC to work</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K60F120M-getting-the-DAC-to-work/m-p/435801#M3918</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please, be sure to select the correct voltage reference for DAC. According to K60's reference manual, you can chose between two different Voltage Reference: Internal reference that is obtained from VREF_OUT and External Reference that is obtained from VDDA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made a simple example using PEx and selected the External Reference and DAC is working without problems. (For Internal reference, you will need to configure VREF)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55911i10FB417D26670BB1/image-size/large?v=v2&amp;amp;px=999" title="DAC reference voltage.jpg" alt="DAC reference voltage.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I attach this basic example,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this can help you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Isaac&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Sep 2015 19:36:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K60F120M-getting-the-DAC-to-work/m-p/435801#M3918</guid>
      <dc:creator>isaacavila</dc:creator>
      <dc:date>2015-09-10T19:36:27Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60F120M getting the DAC to work</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K60F120M-getting-the-DAC-to-work/m-p/435802#M3919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Isaac,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks, that actually was the only problem. The default was using the internal reference which I did not change. But why is VREF_OUT not configured?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Jan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Sep 2015 09:45:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K60F120M-getting-the-DAC-to-work/m-p/435802#M3919</guid>
      <dc:creator>jrs1986</dc:creator>
      <dc:date>2015-09-11T09:45:03Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60F120M getting the DAC to work</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K60F120M-getting-the-DAC-to-work/m-p/435803#M3920</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;VREF_OUT is not configured because it is necessary to add this module and configure apart. This is done because VREF_OUT is not only used for DAC but it is also used for ADC module and others.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So basically, if you need to select VREF_OUT as reference voltage for DAC, you will need to add this component and configure it as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56029iADBC7B1A07D0D9E3/image-size/large?v=v2&amp;amp;px=999" title="Configure VREF.jpg" alt="Configure VREF.jpg" /&gt;&lt;/span&gt;I hope this can help you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Isaac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Sep 2015 13:20:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/TWR-K60F120M-getting-the-DAC-to-work/m-p/435803#M3920</guid>
      <dc:creator>isaacavila</dc:creator>
      <dc:date>2015-09-11T13:20:16Z</dc:date>
    </item>
  </channel>
</rss>