<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic how to load program to internal flash in KDS using pe micro in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/how-to-load-program-to-internal-flash-in-KDS-using-pe-micro/m-p/433492#M3863</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt; i am using K60 tower board ..with PE Micro programmer.we load the code using Debug mode........That code is loaded and its running and its working very much.....&lt;/P&gt;&lt;P&gt;when i power off then i power on , the code i loaded using debug mode not running..........&lt;/P&gt;&lt;P&gt;why the code not running is that code loaded into ram....how can i load the code into flash....if that code load into flash why that code not running after restart...&lt;/P&gt;&lt;P&gt;in kds there is no option to load the code into flash...but i have seen in code warrior there is option for ram or flash...................................&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We tried kds 2.0 file to flash but that not working&lt;/P&gt;&lt;P&gt;please tell me its very urgent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Aug 2015 02:18:43 GMT</pubDate>
    <dc:creator>lijofrancis</dc:creator>
    <dc:date>2015-08-12T02:18:43Z</dc:date>
    <item>
      <title>how to load program to internal flash in KDS using pe micro</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/how-to-load-program-to-internal-flash-in-KDS-using-pe-micro/m-p/433492#M3863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt; i am using K60 tower board ..with PE Micro programmer.we load the code using Debug mode........That code is loaded and its running and its working very much.....&lt;/P&gt;&lt;P&gt;when i power off then i power on , the code i loaded using debug mode not running..........&lt;/P&gt;&lt;P&gt;why the code not running is that code loaded into ram....how can i load the code into flash....if that code load into flash why that code not running after restart...&lt;/P&gt;&lt;P&gt;in kds there is no option to load the code into flash...but i have seen in code warrior there is option for ram or flash...................................&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We tried kds 2.0 file to flash but that not working&lt;/P&gt;&lt;P&gt;please tell me its very urgent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 02:18:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/how-to-load-program-to-internal-flash-in-KDS-using-pe-micro/m-p/433492#M3863</guid>
      <dc:creator>lijofrancis</dc:creator>
      <dc:date>2015-08-12T02:18:43Z</dc:date>
    </item>
    <item>
      <title>Re: how to load program to internal flash in KDS using pe micro</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/how-to-load-program-to-internal-flash-in-KDS-using-pe-micro/m-p/433493#M3864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the linker file *.ld decide the memory allocation. please check if you use the right ld file and if the code is allocated in Flash in your ld file.&lt;/P&gt;&lt;P&gt;see attached for where to check the ld file configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can this help?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 02:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/how-to-load-program-to-internal-flash-in-KDS-using-pe-micro/m-p/433493#M3864</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-08-12T02:42:23Z</dc:date>
    </item>
  </channel>
</rss>