<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Grouping components in KDS(processor expert)</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Grouping-components-in-KDS-processor-expert/m-p/433342#M3858</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is it possible to group a set of components in KDS?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For example ,if i have an SPI_MasterLDD and a couple of Bit IOs LDD,can i group them into one and later if i add the group the same components with the same settings can be used in any future projects?&lt;/P&gt;&lt;P&gt;Note:I do not want to create a new component all together,just to group them into one single unit.&lt;/P&gt;&lt;P&gt;I really like processor expert ,but it would be really helpful if there was a simple button to do this.&lt;/P&gt;&lt;P&gt;Just select all the components you want to group(in the components view),right click and there should be an option "group" or something similar.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In code warrior ,we have a similar setting.When you right click on the component we get an option "Save component settings as template" which is missing in KDS&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Oct 2015 06:21:38 GMT</pubDate>
    <dc:creator>arunkumar1989</dc:creator>
    <dc:date>2015-10-28T06:21:38Z</dc:date>
    <item>
      <title>Grouping components in KDS(processor expert)</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Grouping-components-in-KDS-processor-expert/m-p/433342#M3858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is it possible to group a set of components in KDS?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For example ,if i have an SPI_MasterLDD and a couple of Bit IOs LDD,can i group them into one and later if i add the group the same components with the same settings can be used in any future projects?&lt;/P&gt;&lt;P&gt;Note:I do not want to create a new component all together,just to group them into one single unit.&lt;/P&gt;&lt;P&gt;I really like processor expert ,but it would be really helpful if there was a simple button to do this.&lt;/P&gt;&lt;P&gt;Just select all the components you want to group(in the components view),right click and there should be an option "group" or something similar.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In code warrior ,we have a similar setting.When you right click on the component we get an option "Save component settings as template" which is missing in KDS&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 06:21:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Grouping-components-in-KDS-processor-expert/m-p/433342#M3858</guid>
      <dc:creator>arunkumar1989</dc:creator>
      <dc:date>2015-10-28T06:21:38Z</dc:date>
    </item>
    <item>
      <title>Re: Grouping components in KDS(processor expert)</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Grouping-components-in-KDS-processor-expert/m-p/433343#M3859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;you can put components into groups/folders. Create a group/folder with the context menu:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25539i0B4B766169455180/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Use File &amp;gt; Export to export component settings:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25621i5B8851F0D85D9201/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;See &lt;A href="http://mcuoneclipse.com/2014/10/26/export-and-import-processor-expert-component-settings/" title="http://mcuoneclipse.com/2014/10/26/export-and-import-processor-expert-component-settings/"&gt;Export and Import Processor Expert Component Settings | MCU on Eclipse&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 07:01:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Grouping-components-in-KDS-processor-expert/m-p/433343#M3859</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-10-28T07:01:15Z</dc:date>
    </item>
  </channel>
</rss>