<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: pre loaded code not running after power on using kinetis design studio in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/pre-loaded-code-not-running-after-power-on-using-kinetis-design/m-p/431818#M3781</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Lijo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend you first test on simple project , please see the attachment,&amp;nbsp; it is create on TWR-K60D10M board,&lt;/P&gt;&lt;P&gt;and the function of the project is light the LED , please download&amp;nbsp; it , and the power off , then power on to test .&lt;/P&gt;&lt;P&gt;I have test it on my side ,it can work well when re-power on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Aug 2015 02:46:37 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2015-08-12T02:46:37Z</dc:date>
    <item>
      <title>pre loaded code not running after power on using kinetis design studio</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/pre-loaded-code-not-running-after-power-on-using-kinetis-design/m-p/431817#M3780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;I am using Kinetis Design studio 2.0 with update,and we use K60 towerboard.i load the code using the mode debug as....its working....&lt;/P&gt;&lt;P&gt;my code running successfully......&lt;/P&gt;&lt;P&gt;But my problem is that after i power off the tower board then power on ,the code not running.......&lt;/P&gt;&lt;P&gt;is that code load into ram ? not flash?....&lt;/P&gt;&lt;P&gt;why that code not running after power restart?&lt;/P&gt;&lt;P&gt;How the&amp;nbsp; code, we loaded has gone?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in KDS we checked flash from file that not working.....................................&lt;/P&gt;&lt;P&gt;programmer we use Pe Micro....please tell me how to resolve my problem&lt;/P&gt;&lt;P&gt;Please tell me its very urgent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 18:03:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/pre-loaded-code-not-running-after-power-on-using-kinetis-design/m-p/431817#M3780</guid>
      <dc:creator>lijofrancis</dc:creator>
      <dc:date>2015-08-11T18:03:07Z</dc:date>
    </item>
    <item>
      <title>Re: pre loaded code not running after power on using kinetis design studio</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/pre-loaded-code-not-running-after-power-on-using-kinetis-design/m-p/431818#M3781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Lijo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend you first test on simple project , please see the attachment,&amp;nbsp; it is create on TWR-K60D10M board,&lt;/P&gt;&lt;P&gt;and the function of the project is light the LED , please download&amp;nbsp; it , and the power off , then power on to test .&lt;/P&gt;&lt;P&gt;I have test it on my side ,it can work well when re-power on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 02:46:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/pre-loaded-code-not-running-after-power-on-using-kinetis-design/m-p/431818#M3781</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-08-12T02:46:37Z</dc:date>
    </item>
  </channel>
</rss>