<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: Converting code to the KDS environment</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Converting-code-to-the-KDS-environment/m-p/428186#M3613</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not aware of any document like that.&lt;/P&gt;&lt;P&gt;You can create a sample project with the wizard to be compliant with your hardware configuration.&lt;/P&gt;&lt;P&gt;The example will include all configuration to build and load the sample code on your board.&lt;/P&gt;&lt;P&gt;After that you can use this project and add your files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the community there are some posts explaining how to convert project from X dev tool (as CW for MCU V10.x) to KDS.&lt;/P&gt;&lt;P&gt;Under the KDS installation you can refer to the manuals (\KDS_3.0.0\doc)&lt;/P&gt;&lt;P&gt;&amp;nbsp; - KDS_Porting_Guide.pdf&lt;/P&gt;&lt;P&gt;&amp;nbsp; - KDS_Users_Guide.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Under KSDK there are some documentations too under \KSDK_1.3.0\doc folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Oct 2015 10:23:30 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2015-10-27T10:23:30Z</dc:date>
    <item>
      <title>Converting code to the KDS environment</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Converting-code-to-the-KDS-environment/m-p/428185#M3612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wrote a project in C on top of Ubunto which I need to run on top of the K64F, I already installed KDS 3.0.0 as well as KSDK 1.3.0 and the SEGGER J_LInk&lt;/P&gt;&lt;P&gt;1. Is there a automatic tool that can help me to do the conversion?&lt;/P&gt;&lt;P&gt;2. What are the steps I need to do in order to complete the task?&lt;/P&gt;&lt;P&gt;3. What are the necessary changes I need to do (e.g. printf)?&lt;/P&gt;&lt;P&gt;4. Is there is any good tutorial for the KDS?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Oct 2015 09:54:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Converting-code-to-the-KDS-environment/m-p/428185#M3612</guid>
      <dc:creator>rasa</dc:creator>
      <dc:date>2015-10-26T09:54:03Z</dc:date>
    </item>
    <item>
      <title>Re: Converting code to the KDS environment</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Converting-code-to-the-KDS-environment/m-p/428186#M3613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not aware of any document like that.&lt;/P&gt;&lt;P&gt;You can create a sample project with the wizard to be compliant with your hardware configuration.&lt;/P&gt;&lt;P&gt;The example will include all configuration to build and load the sample code on your board.&lt;/P&gt;&lt;P&gt;After that you can use this project and add your files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the community there are some posts explaining how to convert project from X dev tool (as CW for MCU V10.x) to KDS.&lt;/P&gt;&lt;P&gt;Under the KDS installation you can refer to the manuals (\KDS_3.0.0\doc)&lt;/P&gt;&lt;P&gt;&amp;nbsp; - KDS_Porting_Guide.pdf&lt;/P&gt;&lt;P&gt;&amp;nbsp; - KDS_Users_Guide.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Under KSDK there are some documentations too under \KSDK_1.3.0\doc folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Oct 2015 10:23:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Converting-code-to-the-KDS-environment/m-p/428186#M3613</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-10-27T10:23:30Z</dc:date>
    </item>
  </channel>
</rss>