<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: PWM component in PE for KDS?</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/PWM-component-in-PE-for-KDS/m-p/426602#M3542</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason,&lt;/P&gt;&lt;P&gt;Attached is example using KDS_3.0+KSDK_1.3 for FRDM-K64F that is using GPIO, FTM0, and FTM3.&lt;/P&gt;&lt;P&gt;FTM0 PWM duty cycle is going from 0-100 to see the Green LED change when jumper J1-pin 5 connects to J2-pin 2.&lt;/P&gt;&lt;P&gt;FTM0 PWM duty cycle is going from 100-0 and can be seen on J2-pin 10 (optionally connect it to R68 of RED LED) on o-scope.&lt;/P&gt;&lt;P&gt;The GPIO is used to toggle Green LED every 15 seconds.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Nov 2015 20:21:32 GMT</pubDate>
    <dc:creator>DavidS</dc:creator>
    <dc:date>2015-11-19T20:21:32Z</dc:date>
    <item>
      <title>PWM component in PE for KDS?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/PWM-component-in-PE-for-KDS/m-p/426601#M3541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a K64 processor.&amp;nbsp; In the processor expert that's part of Codewarrior (10.6) there was a PWM LDD that I was using to generate a square wave.&amp;nbsp; It used FTM3 and output the square wave out of the PTD3/FTM3_CH3 pin.&amp;nbsp; Is there a comparable component in the processor expert that comes with KDS?&amp;nbsp; I've looked, but I can't seem to find it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Nov 2015 13:07:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/PWM-component-in-PE-for-KDS/m-p/426601#M3541</guid>
      <dc:creator>jasonpionke</dc:creator>
      <dc:date>2015-11-19T13:07:27Z</dc:date>
    </item>
    <item>
      <title>Re: PWM component in PE for KDS?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/PWM-component-in-PE-for-KDS/m-p/426602#M3542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason,&lt;/P&gt;&lt;P&gt;Attached is example using KDS_3.0+KSDK_1.3 for FRDM-K64F that is using GPIO, FTM0, and FTM3.&lt;/P&gt;&lt;P&gt;FTM0 PWM duty cycle is going from 0-100 to see the Green LED change when jumper J1-pin 5 connects to J2-pin 2.&lt;/P&gt;&lt;P&gt;FTM0 PWM duty cycle is going from 100-0 and can be seen on J2-pin 10 (optionally connect it to R68 of RED LED) on o-scope.&lt;/P&gt;&lt;P&gt;The GPIO is used to toggle Green LED every 15 seconds.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Nov 2015 20:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/PWM-component-in-PE-for-KDS/m-p/426602#M3542</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2015-11-19T20:21:32Z</dc:date>
    </item>
  </channel>
</rss>