<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: Error in KDS</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Error-in-KDS/m-p/426285#M3521</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi dona,&lt;/P&gt;&lt;P&gt;can you shar a screenshot? I believe this is a message coming from the Segger J-Link debug firmware, and is not an error, but an information message. You can tell the Segger J-Link GDB server if it shall use little or big endian, and by default the firmware selects it automatically based on the device used, which is little endian for ARM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Jun 2015 10:39:26 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2015-06-24T10:39:26Z</dc:date>
    <item>
      <title>Error in KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Error-in-KDS/m-p/426284#M3520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When I run aprogram in KDS ,the following error shows up.&lt;/P&gt;&lt;P&gt;"The target endianness is set automatically (currently little endian) "&lt;/P&gt;&lt;P&gt;Why does this error occur? Please help.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Dona&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 09:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Error-in-KDS/m-p/426284#M3520</guid>
      <dc:creator>donad</dc:creator>
      <dc:date>2015-06-24T09:46:59Z</dc:date>
    </item>
    <item>
      <title>Re: Error in KDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Error-in-KDS/m-p/426285#M3521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi dona,&lt;/P&gt;&lt;P&gt;can you shar a screenshot? I believe this is a message coming from the Segger J-Link debug firmware, and is not an error, but an information message. You can tell the Segger J-Link GDB server if it shall use little or big endian, and by default the firmware selects it automatically based on the device used, which is little endian for ARM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 10:39:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Error-in-KDS/m-p/426285#M3521</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-06-24T10:39:26Z</dc:date>
    </item>
  </channel>
</rss>