<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: Specifying linker section</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Specifying-linker-section/m-p/320802#M329</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah, thank you Erich.&amp;nbsp; Being able to turn off the code generation when it's not wanted could be useful, and that's exactly what I need to be able to control the linker sections.&amp;nbsp; Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Jul 2014 12:47:49 GMT</pubDate>
    <dc:creator>davidsherman</dc:creator>
    <dc:date>2014-07-16T12:47:49Z</dc:date>
    <item>
      <title>Specifying linker section</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Specifying-linker-section/m-p/320798#M325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the GCC documentation, if I add __attribute__((section("section name")) to a declaration, I can specify a section.&amp;nbsp; However, the linker file has warnings saying don't touch it.&amp;nbsp; I don't see any settings under the project properties for locating sections.&amp;nbsp; How does one specify a specific location for something?&amp;nbsp; I'm using Processor Expert, so that's where the warning not to edit the linker file comes from.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jul 2014 01:19:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Specifying-linker-section/m-p/320798#M325</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2014-07-16T01:19:58Z</dc:date>
    </item>
    <item>
      <title>Re: Specifying linker section</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Specifying-linker-section/m-p/320799#M326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;did you define the section in ld file?&lt;/P&gt;&lt;P&gt;please refer &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="2020" data-containertype="14" data-objectid="101437" data-objecttype="102" href="https://community.freescale.com/docs/DOC-101437"&gt;https://community.freescale.com/docs/DOC-101437&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"2.1 . No fill() command involved."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this works on my side without any error.&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;====================================================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this answer is for you. if it helps, please click on "correct answer" button. thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;ZhangJun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jul 2014 02:23:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Specifying-linker-section/m-p/320799#M326</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2014-07-16T02:23:16Z</dc:date>
    </item>
    <item>
      <title>Re: Specifying linker section</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Specifying-linker-section/m-p/320800#M327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;At the top of the ld file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* ################################################################### */&lt;/P&gt;&lt;P&gt;/*##&lt;/P&gt;&lt;P&gt;/*##&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; THIS COMPONENT MODULE IS GENERATED BY THE TOOL. DO NOT MODIFY IT. */&lt;/P&gt;&lt;P&gt;/*##&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; */&lt;/P&gt;&lt;P&gt;/*##&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Filename&amp;nbsp; : ProcessorExpert.ld */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, if I modify the file and ProcessorExpert overwrites it if I change something, how does one specify the section that makes Processor Expert aware of it?&amp;nbsp; I have confirmed that PE overwrites the ld file, removing my edits.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jul 2014 12:17:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Specifying-linker-section/m-p/320800#M327</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2014-07-16T12:17:41Z</dc:date>
    </item>
    <item>
      <title>Re: Specifying linker section</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Specifying-linker-section/m-p/320801#M328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can disable the linker file generation, see last dialog in &lt;A href="http://mcuoneclipse.com/2012/03/23/disable-my-code-generation/" title="http://mcuoneclipse.com/2012/03/23/disable-my-code-generation/"&gt;Disable my Code Generation | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jul 2014 12:29:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Specifying-linker-section/m-p/320801#M328</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-07-16T12:29:38Z</dc:date>
    </item>
    <item>
      <title>Re: Specifying linker section</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Specifying-linker-section/m-p/320802#M329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah, thank you Erich.&amp;nbsp; Being able to turn off the code generation when it's not wanted could be useful, and that's exactly what I need to be able to control the linker sections.&amp;nbsp; Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jul 2014 12:47:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Specifying-linker-section/m-p/320802#M329</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2014-07-16T12:47:49Z</dc:date>
    </item>
  </channel>
</rss>