<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: KBOOT V1.2 LED demo application</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414917#M3145</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christie，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in KBOOT, under FSL_Kinetis_Bootloader_1_2_0\FSL_Kinetis_Bootloader_1_2_0\targets, it includes KDS project.&lt;/P&gt;&lt;P&gt;however, FSL_Kinetis_Bootloader_1_2_0\apps is for IAR project only,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so far, there is not an importer to port the IAR or Keil project to KDS directly. users have to create a KDS project with wizard then port the code from IAR project file by file, part by part.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can refer this link for how to generate bin file:&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2014/04/20/binary-files-for-the-mbed-bootloader-with-eclipse-and-gnu-arm-eclipse-plugins/" title="http://mcuoneclipse.com/2014/04/20/binary-files-for-the-mbed-bootloader-with-eclipse-and-gnu-arm-eclipse-plugins/"&gt;Binary (and S19) Files for the mbed Bootloader with Eclipse and GNU ARM Eclipse Plugins | MCU on Eclipse&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can this help?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Aug 2015 06:58:17 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2015-08-06T06:58:17Z</dc:date>
    <item>
      <title>KBOOT V1.2 LED demo application</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414915#M3143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using KDS 3.0.0 to try the led demo application in KBOOT V1.2 release. It looks like that it is built on IAR, not KDS 3.0.0, Is it true?&lt;/P&gt;&lt;P&gt;If so, how to test on KDS 3.0.0? What is the settings for KDS 3.0.0 environment to test led demo application?&lt;/P&gt;&lt;P&gt;Another question: I can't find a way to generate *.bin file in KDS 3.0.0, only *.elf, and *.srec files. Could you tell me how to generate *.bin file by using KDS 3.0.0?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2015 13:25:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414915#M3143</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2015-08-05T13:25:09Z</dc:date>
    </item>
    <item>
      <title>Re: KBOOT V1.2 LED demo application</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414916#M3144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Christis ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1)&amp;nbsp; From the Kinetis Bootloader v1.2.0 Release Notes.pdf , we can see that KBOOT v1.2&amp;nbsp; can&amp;nbsp; compile on KDS 3.0 .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55541i583DAD3E4EAFCB37/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;(2) On KDS 3.0, please configure here to generate .bin file :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55572i28926E41CC036503/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55593i2264F11E4F050F9A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then build , you find the .bin file under the debug file .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 02:26:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414916#M3144</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-08-06T02:26:12Z</dc:date>
    </item>
    <item>
      <title>Re: KBOOT V1.2 LED demo application</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414917#M3145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christie，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in KBOOT, under FSL_Kinetis_Bootloader_1_2_0\FSL_Kinetis_Bootloader_1_2_0\targets, it includes KDS project.&lt;/P&gt;&lt;P&gt;however, FSL_Kinetis_Bootloader_1_2_0\apps is for IAR project only,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so far, there is not an importer to port the IAR or Keil project to KDS directly. users have to create a KDS project with wizard then port the code from IAR project file by file, part by part.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can refer this link for how to generate bin file:&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2014/04/20/binary-files-for-the-mbed-bootloader-with-eclipse-and-gnu-arm-eclipse-plugins/" title="http://mcuoneclipse.com/2014/04/20/binary-files-for-the-mbed-bootloader-with-eclipse-and-gnu-arm-eclipse-plugins/"&gt;Binary (and S19) Files for the mbed Bootloader with Eclipse and GNU ARM Eclipse Plugins | MCU on Eclipse&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can this help?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 06:58:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414917#M3145</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-08-06T06:58:17Z</dc:date>
    </item>
    <item>
      <title>Re: KBOOT V1.2 LED demo application</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414918#M3146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you. Now, I can generate *.bin file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is now that I loaded *.bin file to K64F by using bootloader, it didn't work.&lt;/P&gt;&lt;P&gt;I tried the demo *.bin file and works fine.&lt;/P&gt;&lt;P&gt;I changed the link file for my project and check the required address, looks fine. But, it didn't work.&lt;/P&gt;&lt;P&gt;See attached *.s19 file for the address allocation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone tell me how to set memory section in order to work with bootloader?&lt;/P&gt;&lt;P&gt;I am using KDS 3.0.0, KSDK1.0.0, and PE for my project...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 12:45:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414918#M3146</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2015-08-06T12:45:31Z</dc:date>
    </item>
    <item>
      <title>Re: KBOOT V1.2 LED demo application</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414919#M3147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the following questions when I use KDS3.0.0 to generate *srec file:&lt;/P&gt;&lt;P&gt;Here is the header in *.srec file&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Courier New';"&gt;S00B00006956542E7372656306&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Courier New';"&gt;S21400A00000000320D9A40000E9A40000E9A4000091&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Courier New';"&gt;S21400A010E9A40000E9A40000E9A400000000000094&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Courier New';"&gt;S21400A020000000000000000000000000E9A400009E&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Courier New';"&gt;S21400A030E9A4000000000000E9A40000E9A4000074&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Courier New';"&gt;-----Stack top ==0x2003_0000, Reset_Handler==0x0000_A4D9, DebugMon_Handler==0x0000_A4E9&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Courier New';"&gt;But, in map file it shows as follows:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; .text&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000a4d8&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x14 ./SDK/platform/devices/MK64F12/startup/gcc/startup_MK64F12.o&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000a4d8&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Reset_Handler&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000a4e8&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DebugMon_Handler&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000a4e8&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I2C0_IRQHandler&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000a4e8&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; HardFault_Handler&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that the address in map file is right...Could you tell me where the problem is? *.srec file is right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 18:28:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414919#M3147</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2015-08-06T18:28:54Z</dc:date>
    </item>
    <item>
      <title>Re: KBOOT V1.2 LED demo application</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414920#M3148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anyone who can answer my question:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The interrupt address in *.srec file is ended with odd address, but in map file is ended with even address?&lt;/P&gt;&lt;P&gt;I tried to generate S3 and got the same result? The *.srec file is right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2015 20:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414920#M3148</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2015-08-07T20:26:35Z</dc:date>
    </item>
    <item>
      <title>Re: KBOOT V1.2 LED demo application</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414921#M3149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi Christie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this is the ARM Thumb bit: function pointers (and vectors pointers) have the Thumb bit set in the address, to mark that they are thumb functions.&lt;/P&gt;&lt;P&gt;So it is because of the ARM Thumb mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2015 02:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KBOOT-V1-2-LED-demo-application/m-p/414921#M3149</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-08-10T02:29:45Z</dc:date>
    </item>
  </channel>
</rss>